Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82864A Hi,
My customer has the following requirements: Input voltage: 3.3V, output voltage: 0.9V, rated current: 4A, output voltage ripple :0.2% of Vout
My questions are:
1. Do we have a power module…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82864A , TPSM82810 Hello,
I am designing a board whose delivery times to the customer are short. Therefore I am trying to find a DC2DC in stock that can work with the XILINX ZU7EV. There are currently…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82866A , TPSM82864A , Dear Specialists,
My customer is considering LMZM30604 and has a question.
I would be grateful if you could advise.
---
I'd like to use multiple LMZ30604s.
According to…
Part Number: TPS84410 Other Parts Discussed in Thread: LMZ30604 Hello TI experts,
Are TPS84410 and LMZ30604 the same?
there are no differences between these 2 parts, including package, pin map, block diagram, even electric characteristics.
Please confirm…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82866A , TPSM82864A , SN74HCS05 Dear Specialists,
Our customer has a question.
---
INH pin of LMZ30604 has Pull Up and Pull Down resistor in the device.
Could you please let us know the value of…
Part Number: LMZ30604 Dir,
I have a question about slow start time of LMZ30603 (power modeule ).
Is it possible to set slow start time less than 1.1msec?
I'd like to know that the LMZ30603 can be set a slow start time with STSEL=OPEN and SS/TR=External…
Part Number: LMZ30604 Other Parts Discussed in Thread: SN74LVC1G04 , Hi,
In our power sequencer circuit, We are connecting the output of SN74LVC1G04 buffer to INH/UVLO pin of LMZ30604.
The datasheet has the following note: "Use an open drain or open collector…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPS84610 , Hello Sir/Mam
We require LMZ30604RKGT part detailed land pattern as in datasheet the information for pins 37,38 and 39 is not given . it is written that thermal pin size and shape shown on…
Part Number: LMZ30604 Other Parts Discussed in Thread: SN74LVC1G04 , In customer power sequencer circuit, They are connecting the output of SN74LVC1G04 buffer to INH/UVLO pin of LMZ30604.
The datasheet has the following note: "Use an open drain or open collector…
Part Number: LMZ30604 Hi,
I understand that the efficiency curve was taken by using EVM and so we can see the similar result if we measure the efficiency by using EVM. Then how much variation can be seen between each EVM? Please give your rough estimation…