Part Number: LMZ30606 In the situation of concern, the power good pin is pulled-up to 3.3V through 20kohms and there is a 0.1uF capacitor connected to ground.
The abs max current for the PG pin is 10mA. Is there any chance of damage to the LMZ30606 device…
Part Number: LMZ30606 Hello,
looking for the dimensions of pins 37, 38 and 39 on the part LMZ30606. The drawing for that part says the thermal pin size and shape are shown on a separate sheet. I am not able to locate this document, are you able to help…
Part Number: LMZ30606 Hello,
I'm using the TPS7A8701 connected to LMZ30606.
I wish to connect the PGOOD of the TPS7A8701 to the LMZ30606.
Is it possible to connect it to the INH/UVLO pin ?
Should we use any pull up resistor on this pin ?
Can you please…
Part Number: LMZ30606EVM-003 Other Parts Discussed in Thread: TPS84610 , , LMZ30606 I am doing a failure test for the LMZ30606 6A Power Module using the evaluation board LMZ30606EVM-003. The evaluation board's IC marking say "TPS84610" instead of the expected…
Part Number: LMZ30606 We have designed this part into one of our products. We have had 2 customer returns with the same failure. Basically there's a pretty catastrophic short between the following pins: VOUT, PH, VIN, AGND. Obviously that's very bad…
Part Number: LMZ30606 Hello Team,
We have a problem in using LMZ30606:
We convert 5V to 3.3V by using this chip, and we found that there is no output.
At beginning we thought maybe the INH signal(as red block show) is wrong, and we cut this signal…
Part Number: LMZ30606 Hi,
The specification sheet for this part does not have the dimensions for all pads. The 3 center pads have a note pointing to another sheet, but the other sheet does not exist. Where can I find those dimensions? Thanks in advance…
Part Number: LMZ30606 Hi.
Pin 37 dimension is 1.6X1.6mm
in page 31, layout example it is shown the pin and a 2.8mmX2.8mm square with thermal vias.
my questions are:
1. my pcb editor built the pad as a 2.8mmX2.8mm and solder mask opening of 1.6X1.6 mm…
Part Number: LMZ30606 Team,
A customer of mine would like to operate the LMZ30606 without any electrolytic capacitors, just ceramic capacitors.
The goal is to implement an input filter to the LMZ30606, likely a series damped LC filter. Below are some…