Part Number: LMZ31506 used two LMZ31506,frist LMZ31506 PWRGD pin could drive the second LMZ31506 INH/UVLO?
INH/UVLO pin could direct connect PWRGD pin?
Part Number: LMZ31506 I designed 9.16 Slow Start (SS/TR) in the LMZ31506 data sheet with Css=4700pF (±10%) and SS time=2.8ms, but the power startup result is 2.2041ms. (See attached waveform)
Even taking into account the error of the capacitor, the…
Part Number: LMZ31506 Other Parts Discussed in Thread: TPS84621 , TPS84620 , TPS82130 LMZ31506のスロースタートについて教えてください。
LMZ31506のデータシートの9.16 Slow Start (SS/TR)にて、時間とコンデンサの定数の関係についてTable6に記載されていますが、計算方法はどこに記載されていますか?
データシートは下記リンクを参照しております。 www.ti.com/.…
Part Number: LMZ31506 We're using an LMZ31506RUQ to generate 1.0V from 5.0V - which it is doing - and then using the PWRGD output of that device to enable 2 LMZ31503RUQ's,1 LMZ31503RUQ, and 1 TPS7A8801RTJ. However, the outputs of these sequenced devices…
Part Number: LMZ31506 The board was working fine, but at some point the LMZ31506RUQR's VOUT output (+3.3V) went to 0V.
・When I measured the resistance value between VOUT and GND after it became 0V, it was 1.9Ω. ・The resistance value between VOUT and…
Part Number: LMZ31506 Hi,
I have built a PCB where a LMZ31506 powers the circuit. The schematic and the layout I found in the datasheet. Inputvoltage is 12V and outputvoltage is 5 V. After applying power to the PCB the outputvoltage of the LMZ31506…
Part Number: LMZ31506 When LMZ31506 startup, power good output is delayed about 6ms.
Please refer below waveform;
※ch1: Vin (5V), ch2: Vout (1.03V), ch3: PWRGD
Is there any reason for PWRGD delay?
If there detailed schematic, please let me e…
Part Number: LMZ31506 Other Parts Discussed in Thread: LMZ31710 , Can INH / UVLO pins be used with 0V / + 3.3V active controls (CPLDs, power sequencers, etc.) instead of open drains?
In this case, a pull-down resistor (about 1k to 10kΩ) is connected…
Part Number: LMZ31506 Other Parts Discussed in Thread: LMZ31503 , TPS54320 Greetings, we are attempting to track a 1.8V turn on (LMZ31506) to a 3.3V turn on (LMZ31503). The resistors we've calculated are R1 = 37.8K and R2 = 18.9K. Unfortunately this results…
Part Number: LMZ31506 Hi
Are the below three parts drop in replacement for one another
I am designing a 12 to 5V converter
Can I mount any of these for a common circuit
TPS84621RUQT
LMZ31506RUQT
LMZ31506HRUQT
…