Part Number: LMZ31520LMZ31520RLGT being used to source 0.9V core voltage for Stratix FPGA. Module goes bad ( No output) after couple of months.
Input is 12V, Output 0.9V, Max current drawn is 6A.
Switching frequwncy being used is 500MHz. Input 12V…
Part Number: LMZ31520 HI,
The design schematic diagram of LMZ31520 is shown below. Could you please help check if there are any issues? Or good advice?
Thanks!
Part Number: LMZ31520 We received LMZ31520 with package Exceeding Floor Life by > 72 hours , but Height of LMZ31520 is 5.9mm, and it exceeds the maxim height of 4.5mm defined in Tabel 4-1 of J-STD-033D. What's TI's suggestion about bake time for these…
Part Number: LMZ31520 Other Parts Discussed in Thread: LMZ31530 Hello, Due to delivery issue recently, my customer plans to replace LMZ31530 by LMZ31520, since Iout(max) = <20A at their design. They would like to adjust current limit so that it will be…
Part Number: LMZ31520 Hello,
My customer has a question about the stability analysis of TI power module.
Are there any parts that may cause stability issues among the TI power module products below? What part is it?
LMZ31520RLGT LMZ31710RVQR LMZ31707RVQR…
Part Number: LMZ31520 Hi,
Our Operations team would like to do some basic functionality tests of unassembled MZ31520, i.e. outside a PCB, as standalone.
We assume they should provide at least Vi, Rset, Ci, Co and some load.
Any suggestion for…
Part Number: LMZ31520 Hi team,
From the functional block diagram, INH of LMZ31520 has internal pull-up and down resistors.
I recognize they will pull-up the INH pin to VIN * 0.4.
In my customer's system, VIN=5V.
My customer would like to pull…
Part Number: LMZ31520 Other Parts Discussed in Thread: LM3880 , Hello,
Is it possible to use the V5V to power 5V external device like LM3880MF?
What is the drive current capacity of V5V?
Regards,
JH