Part Number: LMZ31704 Tool/software: If I sequence LMZ31074 with each other in a serial fashion - connecting the PWRGD pin of device 1 to the INH/UVLO pin of device 2 - do I still need a pullup resistor on PWRGD?
Part Number: LMZ31704 Other Parts Discussed in Thread: UCD90120 Hi, In one of our project we are using LMZ31704 power module (same as ZC706 design). Below design 30th Pin mentioned ALWAYS ENABLED . Is this module requires enable pin for Enable the power…
Part Number: LMZ31704 Other Parts Discussed in Thread: TPS82130 LMZ31704RVQT Don't have ROHS report, Do we have P2P replace part which have ROHS report?
Part Number: LMZ31704 Hi support team,
I have a question about page 21 of SLVSBV8E. "The INH pin has an internal pullup current source, allowing the user to float the INH pin for enabling the device. If an application requires controlling the INH pin…
Part Number: LMZ31704 Other Parts Discussed in Thread: LMZ31710 , LMZ31707 Hi,
For LMZ31704 the max Output Current is spec at 4A, the Current Limit Threshold is spec at 9A if the ILIM left open, does that mean the part can be loaded up to 9A before the…
Part Number: LMZ31704
Tool/software: WEBENCH® Design Tools
Hello
If the output is less than 0.8V, no design is generated in Webench.
How do you provide a reference design at an output below 0.8V?
Best Regards.
Part Number: TPSM863252 Other Parts Discussed in Thread: LMZ31704
Tool/software:
While I'm fairly confident that PG pulls/asserts low when power is GOOD (active low logic) , it isn't explicitly stated (unless I'm just missing it) whether PG is active…
Part Number: LMZ31704 Other Parts Discussed in Thread: TINA-TI I have downloaded whtever unencrypted and other spice model files from ti website, BUt when i tried to import NEW MACRO it is showing some error.
So please give .TSM file for the same.
Part Number: LMZ31704 Hi, LMZ31704 is designed to output dc5V at 3A from dc6V~12v. And we found that output voltage is not 5V, below it.The ouput voltage will change with input. With load improved, the output voltage descrease. could you please give some…