Hi Hayden,
Using the equation that I mentioned above, your application will be in pulse skipping mode if you load it with 325mA.
The LMZ31704 and LMZ31707 also use the same 1uH internal inductor.
Regards,
Jimmy
Part Number: LMZ22008 Other Parts Discussed in Thread: LMZ31710 , LMZ31704 , , LMZ31707 I am looking at these two modules to drive 5V input of an Atom 1.44 GHz up to 1.92 GHzGHz processor board like Lattepanda or Up board .
From what I read, the LM31707…
Hi Tom,
Thanks for your response.
It seemed it is hard to modify feedback resistors of LMZ31704, and thus my customer is considering LM10011 + TPS54320 combination.
But, they found the minimum output voltage of TPS54320 is +0.8V although C6655 requiring…
No, this does not apply to the LMZ31704.
The LMZ31704 has an internal current source on the INH pin. During operation the voltage on the INH pin is typically 2.8V.
Other Parts Discussed in Thread: LMZ31710 , LMZ31530 , LMZ31704 Hello,
What is the maximum acceptable Junction Temperature, Junction-to-case Thermal Resistance (Theta -JC) and Junction-to-ambient Thermal Resistance (Theta - JA) of the following devices …
Please look at the LMZ31710 (10A) / LMZ31707 (7A) / LMZ31704 (4A) family. These devices will require a 5V bias to operate though.
The LMZ30606 (6A) and LMZ30604 (4A) can operate directly from 3.3V.
Other Parts Discussed in Thread: LMZ31704 , TPS82085 , TPS62080 , TPS82130 I have a design where the TPS82085 would be a perfect fit, however, I need the VOUT MIN to be 0.75V instead of the specified 0.80V. I looked at the LMZ31704, but it is at least 3x…
Part Number: LMZ10504 Other Parts Discussed in Thread: LMZ31704 , LM10504 , TPS25925 , TPD1E05U06 when i use the LMZ10504,this module often damaged,the ouput pin has shorted to ground,
the input voltage is 4.5 and the output is 3V3.
please see the schematic…
Hi Teoh,
Yes, the LMZ31704 can safely handle 4A under your operating conditions. Your conditions should result in less than 1W of power dissiaption and greater than 95% efficiency. No problem for this package.
Other Parts Discussed in Thread: LMZ31704 , LMZ31710 Hi, There is a following comment at p12 of LMZ31704's datasheet. (There is a same comment at p12 of LMZ31710's datasheet.) ------------------------------------------------------------------…