Part Number: LMZ34002 Is it possible to use the transient model to run gain and phase plots within PSPICE? If so, do you have recommendations of where to place the AC source as the topology of the LMZ34002 is slightly different compared to traditional…
Part Number: LMZ34002 I am designing a circuit that requires the regulator to be off completely until commanded by an FPGA. I am controlling the inhibit pin with a normally closed solid state relay, such that the INH is pulled low until it's commanded…
Part Number: LMZ34002 To set an output voltage of -15.5V, Webench recommends a 205k resistor for Rset. (11-34V input, -15.5V output, 60C operating temp)
The datasheet specifies using 187k resistor for Rset to get -15.5V output.
See Table 3 of the datasheet…
Part Number: LMZ34002 I am trying to simulate LMZ34002 unencrypted model in PSPICE 17.4 and having issues just running a transient analysis. I get ERROR(ORPSIM-15141): Less than 2 connections at node CLK. In my schematic, I have CLK floating (with a alias…
Part Number: LMZ34002 I have been running simulations in PSPICE for the LMZ34002. When I modified the steady state design to incorporate a load step, I am seeing that the when the step occurs, an overshoot happens and then settles back to -15V. When the…
Part Number: LMZ34002 Other Parts Discussed in Thread: LM2574 , Hello,
I have LMZ34002RKGT DC-DC converter and TPS7A3001MDGNTEP LDO. Should I use heatsink with this parts?
Thank you in advance.
Sincerely,
Behtan Umut Mercan
Part Number: LMZ34002 Other Parts Discussed in Thread: DAC81416 , Greetings community,
I'm currently having a ripple issue using the LMZ3004 as a inverter to generate -12V from a 12V input. It is current limited at 700 mA by a current limiter IC. The -12V…