Part Number: LMZ35003 Please tell me whether LMZ35003RKGT conforms to the following environmental standards?
· RoHS status (10 substances) · REACH status (191 substances) · Green status · IEC 62474
The status of the Web Page is…
Part Number: LMZ35003 I'm looking at the datasheet for the LMz35003.
The Vout pin descriptions say the following
VOUT
10
11
12
13
14
15
39
Output voltage. These pins are connected to the internal output inductor. Connect these…
Part Number: LMZ35003 Hi,
Please let me ask if LMZ35003 hsa limitation of startup time. Actually the customer consider to use input voltage that takes 50msec to 24V. Do you have any concern to such power up of input voltage?
Best Regards,
Satoshi / Japan…
Part Number: TPS84250 Other Parts Discussed in Thread: LMZ35003 Hi,
Theses are two devices that seem identical: TPS84250 & LMZ35003
Both these devices have two ordering options each:
TPS84250RKGR
TPS84250RKGT
LMZ35003RKGR
LMZ35003RKGT
The datasheets…
Part Number: LMZ35003 Hi team,
The datasheet gives the Slow Start Capacitor Values and Slow Start Time on Table 8, I want to know if there is a limit for the soft-start time? If the soft-start time can be longer, for example 100ms?. Is there any equation…
Part Number: LMZ35003LMZ35003 datasheet says below:
The LMZ35003 requires a minimum input capacitance of 4.4 μF of ceramic type. The voltage rating of input capacitors must be greater than the maximum input voltage. The ripple current rating of the capacitor…
Part Number: LMZ35003 Hello support team,
My customer is considering to use a LMZ35003 but the current capability of 2.5A max is not good enough for the target system. So that the customer is thinking to make two parallel connection to get more capability…
Part Number: LMZ35003 Hi team,
Customer inquired that measured UVLO voltages are largely different from calculated values.
① Target : Von = 20V , Voff = 18V (Von-Voff = 2.0V)
Ruvlo1=689.6 kΩ (680K+9.6K)
Ruvlo2=44.5 kΩ (43K+1.5K) with 1%…
Part Number: LMZ35003 Hi, Team
My communicaiton customer is using LMZ35003 in their smart antenna products, to convert 12V to 10V. They want to delay the LMZ35003 start up.
As LMZ35003 is first stage power converter, no MCU can control the INH/UVLO pin…
Part Number: LMZ35003 Hi,
I understand that the inhibit threshold voltage has no hysteresis that means the SS pin voltage will be turned on/off at the same INH pin voltage at the same sample. But I could see some difference turn on and off threshold as…