Part Number: LMZ36002 Section 6.5 defines the UVLO thresholds as 3.2V nominal (rising Pvin) and 2.8V nominal (falling Pvin). Section 6.5 defines the INH threshold to be 2.1V nominal. Table 10 shows typical resistor values when using the UVLO feature,…
Part Number: LMZ36002 Hello,
the datasheet of the LMZ36002 only contains the Thermal Pad Mechanical Data, but there is no information about the Land Pattern Data. Where can I find the Board Layout and Stencil Design for RVQ (S-PB3QFN-N43) ?
Andreas
Hi Jimmy
I've made progress on this issue and have isolated the cause of the problem we were experiencing.
In the previous test where INH was tied to PVIN, I reported that the LMZ36002 would shutdown when heated. However, that setup still contained…
Part Number: LMZ36002 Hello team,
Can you help to clarify the purpose of the soldermask defined pads in the LMZ36002 footprint (datasheet page 37)?
My customers design allows via-in-pad, so they would like to eliminate the hatched areas in the image…
Part Number: LMZ36002 TI LMZ36002 is VERY COOL! Thanks TI!
The data sheet provides "allowable" switching frequencies under some described conditions; however, there is no information about the resulting behavior if conditions change and the part is used…
Part Number: LMZ36002 1- Can 2 or more LMZ36002 be run in parallel (either to increase load or fault tolerance)?
2- If 2 devices are run in parallel, should the parts be sync'd with clock at 180 degrees? or each part should run independently?
Tha…
Part Number: LMZ36002
Hi,
I am currently developing a design with the LMZ36002 on it. We need ULVO at 6V.
There's no way to figure out how to properly use the ULVO pin as there are obviously two opposing views stated in the datasheet.
First. Did…
Part Number: LMZ36002 In the datasheet (june 2017) 10.1 Layout guidelines, it is stated : "Keep AGND and PGND seperate from one another. The connection is made internal to the device."
In the LMZ36002EVM user's guide (september 2015) 6 Schematic…