Part Number: LMZM23601 Other Parts Discussed in Thread: LMZM23600 Good morning
We ordered some of these components from Mouser back in March 2026 with a delivery date of 5 days - this was then delayed and today we have now been told its going to be…
Part Number: LMZM23601 I've been using LMZM23601SILT programmed for 1.8V out with a Vin of 32V without any issue before noticing the maximum recomended input voltage is aproximately 20V. Will this eventually damage the chip?
Thanks,
RJJ
Part Number: LMZM23601 I would like to consult with you regarding the LMZM23601SILT DC/DC converter.
The converter is configured to step down 28 V to 12 V and supplies a load current of approximately 0.1 A .
During a short-circuit recovery test ,…
Part Number: LMZM23601 Hi Ti,
We are considering LMZM23601 with the following configuration: Module Type=Adjustable Vin=24V Vout=5V Mode=FPWM
With this configuration, the output may become unloaded. Is this a problem?
Is a bleeder resistor or similar…
Part Number: LMZM23601 Other Parts Discussed in Thread: TPSM365R6 ,
Tool/software:
LMZM23601 is not recommended for new designs but it seems like the replacement part (TPSM365R6) needs two more resistors and a capacitor as minimum requirements. Is…
Part Number: LMZM23601 Hi team,
Customer have a circuit that creates a 4.9V output using LMZM23601SILR (adjustable type), but in thier prototype, they mistakenly installed LMZM23601V3SILR (3.3V fixed type).
Therefore, although it's an irregular usage…
Part Number: LMZM23601 Tool/software: Hello,
I am using LMZM23601 in inverting buck-boost configuration:
Vin: 12V
Vout: -5V @ 0.5A.
I designed the circuit from Webench simulation, now I have the real design as prototype but the -5V output is not…
Part Number: LMZM23601 Other Parts Discussed in Thread: PSPICE-FOR-TI Hi, Dear product line
my customer configure LMZM23601 as a inverting regulator as below figure shows.
then customer find he could not disable LMZM23601 with a FPGA_IO directly…
Part Number: LMZM23601 Hello, would you know the line regulation and load regulation (voltages) for this component? Could you please state the values and guide me to where it is in the specification. I saw something close on page 28, but it is for the…
Part Number: LMZM23601 Tool/software: hi
i am looking fo a poin competible IC for LMZM23601SILR
with highe current rating
the high input voltage doesnt really matter for me i am looking fo arround 15V input to 11 V output