Part Number: LMZM23601 Hello Expert, My customer facing the issue that mounted inductor's inductance is reduced after mounting. Then, I have some questions for this device as below. 1. Is there any limitation from the point of view of damage for inductor…
Part Number: LMZM23601 Hi Team, I am designing a circuit with LMZM23601 in inverting configuration. My required output voltage is -15V. My input is +20V. I am not using the PGOOD functionality. So I just pulled it up to Vin. Can I leave the PGOOD pin floating…
Part Number: LMZM23601 Dear Specialists.
I will use LMZM23601V3SIL for next pruoduct model.
But at the shipping test, caused LMZM23601's output was repeated turn on and off.
I would be grateful if you could advise.
---
Regarding the board using LMZM23601SIL…
Part Number: LMZM23601 Dear specialists,
I'd like to know what happen when Vout > Vin.
The datasheet P.34 9.3 Do's and Don't's, Vout>Vin doesn't allow.
According to the related thread, it may be damage.
But I can understand what…
Part Number: LMZM23601 Other Parts Discussed in Thread: LM53601-Q1 Is there a chip that is used on this module that is available to evaluate? We would like to decide whether to use the device or the module.
Thanks,
Alula Hailu
Part Number: LMZM23601 Tool/software: WEBENCH Design Tools Hi.
We have used LMZM23601 to generate -6V from 12V input
The MODE/SYNC pin was unfortunately connected to Board ground as shown in figure.
Also CBYP is not added in schematic.
The output I…
Part Number: LMZM23601 Other Parts Discussed in Thread: TPSM84203 , Hello,
Context of my question : I’m developping a medical device. I will have a first AC/DC adaptator (external switching power supply) with an ouput of 24VDC as i need to power a stepper…
Part Number: LMZM23601 Hello Guys,
Good day.
Our customer is using the adjustable output version, set to 6V. Unfortunately due to stocks issues they cannot source any of this parts. Therefore, They were wondering if they can use the fixed output 5V version…
Part Number: LMZM23601 Dear Specialists,
My customer is encountering LMZM23601V3SIL's low voltage and overheating.
I would be grateful if you could advise.
---
Regarding the board using LMZM23601V3SIL, the problem that output voltage becomes low and…