Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: LMZM33603EVM Hello,
a customer of mine sent me the following:
"Not sure if it big deal, just to let you know,
There is an little mismatch between the EVM datasheet and the board it self,
http://www.ti.com/lit/ug/snvu565/snvu565.pdf…
Part Number: LMZM33603EVM Other Parts Discussed in Thread: LMZM33603 Customer is asking if LMZM33603EVM drawing 15mA in no load condition is normal?:
If I disable it, the current drawn is 650uA, which is expected, but in case of no load or light load…
Part Number: LMZM33603EVM Other Parts Discussed in Thread: LMZM33603 Hello,team members.
I want a clearer PCB image from the LMZM33603EVM data sheet(figure8,9,10,11).
Because I can't open Gerber data.
Regards
Part Number: LMZM33603EVM Hi team members.
I measure noise with LMZM33603EVM.
The spike noise voltage is higher when the output noise is measured at both ends of the C10 pad than when measured at both ends of the C5. Why is this?
Part Number: LMZM33603EVM Other Parts Discussed in Thread: LMZM33603 , LMZM33606 Hi, Customers are evaluating LMZM33603 using EVM. There is question about the evaluation results.
Evaluation condition is : Vin=24V, Vout=5V, Synchronization input : 400kHz(High…
Part Number: LMZM33603EVM Other Parts Discussed in Thread: LMZM33603 I'd like to design pattern layout of LMZM33603. Where can I get a gerber file of LMZM33603EVM? Please advice.
Part Number: LMZM33603EVM Hi, team.
What is the recommended value when using LMZM33603EVM with 24Vin 1.8Vout?
Rfbt: 8.07 kΩ, Rfbb: 10 kΩ are planned, but is Cff unnecessary?
Does Cout need to be increased?
Best Regards,
Part Number: LMZM33603EVM Other Parts Discussed in Thread: LMZM33603 Hello TI,
Is it possible to add Gerber file of LMZM33603EVM (or LMZM33603EVM)?
I have buy this board and I would like to see footprint&solder paste on this board. I need to zoom on…
Hi Yusuke-san,
You may expect to have higher ESR when using aluminum electrolytic capacitors as opposed to aluminum polymer capacitors. This may impact your stability.
I would recommend using the Webench designer tool on the product folder if you want…
Part Number: LMZM33606 Other Parts Discussed in Thread: LMZM33603 , , , LMZM33603EVM Hi, Customers are considering LMZM33606 and LMZM33603. Customers want to know the specifications described below. 1.The time that LMZM33606/3 follows when synchronized from…