Part Number: LMZM33604 Other Parts Discussed in Thread: LMZ23605 Hi Team,
One of my customer is designing medical project and requested for RoHS3 compliant buck module. The suggested LMZM33604 is non ROHS compliant3, the device is ROHS3 compliant with exemptions…
Part Number: LMZM33604 I intend to use the LMZM33604 for my new power supply design. Is the LMZM33604 EN55011 Class A compliant. Or do I still need additional components to fulfil EN55011 Class A requirements? Thanks!
Part Number: LMZM33604 Could you please give me any advice to synchronize two LMZM33604s (+15/-15V) with an oscillator? The oscillator must support two shifted outputs (0°/180°).
Part Number: LMZM33604 Hello team,
I have questions about input and output capacitor selection written in LMZM33604 datasheet p.17.
Input capacitor selection
Datasheet states minimum 20uF is required.
Is the value of 20uF effective capacitance value…
Part Number: LMZM33604 Hi expert,
Customer download LMZ33604 footprint from ti.com but it's not match DS. We found a same old discussion in the e2e post but downloaded gerber file is LMZ33603 actually. Do you have a correct footprint or evm gerber file…
Part Number: LMZM33604 Hi all,
I'm looking for additional data for the Theta JA vs PCB-Area from 5 to 15 cm². I'll use the LMZM33604, but not at full output poewr and max. ambient temperature of 50°C, looking for the minimum required PCB area to get Rth…
Part Number: LMZM33604 Other Parts Discussed in Thread: LMZ23610 Hi,
Is it possible to sync 2x LMZM33604 modules with one as a master and another as a slave using the SW pin as the output and the SYNC/MODE pin as the input? Datasheet says not to connect…
Part Number: LMZM33604 Hello E2E,
I know that when use the buck DC/DC for negative voltage output, output voltage has rise up to positive side about 0.6V at startup. DC / DC dedicated to negative voltage output does not have voltage rise up. Does LMZM33604…
Part Number: LMZM33604 Other Parts Discussed in Thread: LM25116 , LM5116 , LM5088 , LM25088 , Tool/software: Hi TI Team,
We want to design design power supply DC DC converter for input voltage 12V output voltage -13.5V with 1A output current capability.
…
Part Number: LMZM33604 Other Parts Discussed in Thread: DAC53401 , LM73605 , LM73606 I am trying to control the output voltage of the LMZM33604 by supplying an adjustable voltage to the SS/TRK pin.
It seems to work but I am confused by the results.
The…