Hi Peter
The schematic looks okay to me.
May I know the output capacitance and the load here?
Looks like the output capacitance is charged here and there is very little load to discharge it when the FET is in OFF state due to which you see this Offset…
Part Number: LM5164-Q1 I started designing with WeBench a buck converter using the LM5164QDDARQ1. I changed some values to reducde the part diversity in my overall deisgn (See WebenchDesign and Implemented design). With RRON being 47kOhm 1% 100ppm I would…
Part Number: DLPLCR65EVM Other Parts Discussed in Thread: DLPR900 , DLPLCRC900EVM I cannot switch the operation mode using DLPC900REF-GUI. It is locked at Video Mode. I cannot load any customed images for display. What's more, even when the power is cut off…
Thanks Calan,
Hi Jimmy,
Both TPS22997 and TPS22992 have thermal shutdown that mitigates the risk of overheating - however, what current are you expecting during a short circuit? If the current is very high (rough estimate of 25A instantaneously), there…
Part Number: BQ24070 Hi Garrett,
One more question! For the case of: - no battery present. - there is a load connected to the OUT pins. - the device is powered off. - 10nF cap on DPPM As we've discussed, when the 5V is turned on to VIN, the BQ24070 will think…
Part Number: DRV8244-Q1 Regarding the switching loss equation in note (4) of datasheet 7.5.14, what are the units for each variable? ex.) Psw [W], Iload [A], etc.
Part Number: XTR115 Other Parts Discussed in Thread: XTR117 Hi,
I have tried to set up a 4..20mA analog output signal with the XTR115.
Everything works so far. However, I seem to have EMC problems.
If a walki talki or a consumer is connected nearby…
Hi,
li liu said: I understand that port0 refers to the data on the MCU side, and port1 refers to the data on the external test PC. Then the load calculation of RGMII on the SOC side is the load received by p0 divided by the load sent by p1, right?
No. …
Part Number: TPS2597 Hi All,
I have a question about TPS2597.
TPS2597 is an eFuse, but is it possible to use it like a load switch?
Best Regards, Ishiwata