Part Number: LP-CC2651P3 Other Parts Discussed in Thread: SYSCONFIG Question: as receiver LP-2651P3 receive data only once, and the first byte data of the payload is lost, and the remaining 7 bytes data of the payload are correctly received;
Here…
Hi,
All the CC26xxP devices can deliver up to 20 dBm output power and proprietary RF.
Refer to reference design LP-CC2651P3: https://www.ti.com/lit/zip/swrc375
In order to achieve 20 dBm, The PA section must be supplied by VDDS which is the default…
Part Number: CC2652P Other Parts Discussed in Thread: LP-CC2651P3
Tool/software:
Hello Team,
I am working with a new application and I am using the CC2652P1FRGZR considering the 20dbm PA. So, I have a couple of questions for that:
Does the antenna…
Hello Lekhraj,
I recommend that you submit your design to SIMPLELINK-2-4GHZ-DESIGN-REVIEWS for further review. My quick thoughts are below:
MSP430 TX --> CC2652 RX & CC2652 TX --> MSP430 RX
It looks like nRESET and JTAG_TMS are swapped on the…
Part Number: CC2652P7 Other Parts Discussed in Thread: CC1352P7 , LP-CC1352P7 , LP-CC2652R7 , LP-CC2651P3
Tool/software:
Dear Support,
My customer plan to evaluate CC2652P74T0RGZR with evaluation kit with OTA features. The closest I found is
LP…
Part Number: BP-CC3301 Other Parts Discussed in Thread: CC3301 , CC2674P10 , CC1354P10 , , LP-AM243 , LP-EM-CC1354P10 Tool/software: Dear Sirs:
I donwloaded the cc33xx-mcu-plugin-0.6 from MySecure to test the CC3301 on the CC2674P10.
According to…
Part Number: CC2651R3 Other Parts Discussed in Thread: CC2650 , CC2652R , SIMPLELINK-CC13XX-CC26XX-SDK , , LP-CC2651P3 Does the CC2651 have the exact same RF modem as the CC2650 and CC2652?
Hi Jerry,
Thank you for your assistance.
I have some questions as below,
1. If we do not use 2.4G 5dBm path, I can remove it in my schematic? or, it need to 5dBm path to receiver ?
2. Based on LP-CC2651P3 EVM schematic, when will it switch the…
John,
I have asked Murata to provide further information about suitable replacements for this connector, in case you need the same low profile.
If your space is not as constrained, you could explore the feasibility of using the larger U.FL receptacle…
Hi Daniel,
Thanks for updating! Please clarify the following:
Are you using the latest TIMAC version (1.5.2) with IAR EWARM 7.40.1 (dependency listed in the Release Notes)?
Can you erase all flash memory and run the default MSA example without…