Part Number: LP-EM-CC2340R53 Other Parts Discussed in Thread: CC2650 Used CC2650 Lauchpad for flashing the image to LP-EM-CC2340R53.
Following errror is shown when trrying to flash a hex image
Error connecting to the target: (Error -242 @ 0x0…
Hello Tarun,
I apologize again for the delay here. Upon looking further into this, here are my thoughts:
tarun kaushik said: When a node is removed from the mesh, it becomes unresponsive and requires re-flashing.
In BLE mesh, when a node is removed…
Part Number: LP-EM-CC2340R53 Tool/software: 编译日志为:
[183]makefile:192: recipe for target 'basic_ble_LP_EM_CC2340R53_freertos_ticlang.out' failed [184] undefined first referenced [185] symbol in file [186] --------- ---------------- [187] LL_initRNGNoise…
Part Number: CC2340R5 Other Parts Discussed in Thread: SYSCONFIG , Hello,
I’ve tested the car_node example on the LP-EM-CC2340R53 board, and the program gets stuck in the assert handler due to an OUT_OF_MEMORY error. After checking the memory usage…
Part Number: LP-EM-CC2340R53
Tool/software:
Hello,
I am looking to be able to program a blank CC2340R53 via the serial bootloader (UART). From what I have found, there is some tooling to do so with the SBL tool from one of TI's Github repositories…
Part Number: LP-EM-CC2340R53 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I'm working on the CC2340R53 using the SimpleLink Low Power F3 SDK 9.10.00.83 , and I would like to enable Coded PHY extended advertising (LE Coded PHY, S=2 or S=8…
Part Number: LP-EM-CC2340R53 Other Parts Discussed in Thread: CC2340R5 Tool/software: Hi Team,
we are using the CC2340R453 and need guidance on setting partitions for various regions.
We would appreciate any input to help us get started.
Example…
Part Number: LP-EM-CC2340R53 Tool/software: I'm using the CC2340R53 with the Basic BLE example , and I want to periodically update the BLE advertising data with sensor values.
To do this, I'm using a separate application thread that sets a flag or sends…
Part Number: LP-EM-CC2340R53 Tool/software: Hi,Ti
*SDK:9.12.0.19
I would like to ask what the reason is for the error code 0x16 returned when executing L2CAP_SendSDU()? Is it related to Bug[BLE_LOKI-3583]?(Fixed on SDK9_11_01_19, Key node was out…
Part Number: LP-EM-CC2340R53 Other Parts Discussed in Thread: CC2340R5 Tool/software: Hi Exerts,
in our application, we use the LFOSC instead of LFXT in the design. this application just supports peripheral.
since the LFOSC is not accurate enough…