Part Number: LP-MSPM0G3507 Tool/software: Hello,
I am producing a PWM signal with TIMG12 and using TIMG7 as input capture to measure the period and duty cycle, and it is set as an up-counter.
When a rising edge is detected, the timer value is captured…
Part Number: LP-MSPM0G3507 Tool/software:
Hello I am measuring here a much less time it is maybe in a range of 4 cycles or less rather than 16 cycles for Q16 Format. Because I was not able to read the Bit 8 (1) (compute ongoing) MATHACL->STATUS plus…
Part Number: LP-MSPM0G3507 Tool/software: Hello,
I have a few questions about the steps involved in using the DAC self-calibration feature.
According to the reference manual on page 753, it states that the CTL.AMP bit should be set first, followed…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507 Tool/software: Hi,
I have a question regarding the formula in the reference manual for the temperature sensor. In Chapter 2.2.5, the equations are for a reference voltage of 1.4V…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: MSPM0G3507 Tool/software: Hello,
I have a question regarding MATHACL. I am using it to perform a multiplication operation. According to the RTM, it states that I have to write to MATHACL->OP1…
Part Number: LP-MSPM0G3507 Tool/software: Hello community, I have the following problem with the capture. I would like to perform rising and falling edge detection with the timer 6 interrupt. but this does not work properly for me. The innterupt triggers…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: SYSCONFIG , MSPM0G3507 Tool/software: I have installed sysconfig-1.22.0_3893 and mspm0_sdk_2_03_00_07 in the folders proposed by the tools (c:\ti\..)
When i try to load with sysconfig (Standalone…
Part Number: LP-MSPM0G3507 Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG , MSPM0G3107 Tool/software: Hi,
I am using the G3107 which is custom PCB with XDS110 debugger, Initially I am able to flash and debug it.
After couples of times of flashing…