Part Number: LP2950 Hi,
I'd like to ask about the thread below.
https://e2e.ti.com/support/power-management/f/196/t/819132
Will LP2950 have the same phenomenon?
(If VIN rises quickly, VOUT tracks VIN and overshoots above the nominal output voltage…
Part Number: LP2950 Hi TI LDO team,
Can you confirm this mistake in the LP2950 datasheet - correct should be I_FB = 20nA introduces an error of ~2% ?
Thanks & BR, KF
Part Number: LP2950-N Hi,
I have a customer asking for the formed lead version of the LP950ACZ-5.0/NOPB that comes in a tape and reel package? I am looking through TI.com for the PN but cannot find it. Can you provide any guidance? Thank you!
Part Number: LP2950-N Hi team,
My customer is using LP2950CDTX-3.3/NOPB to covert 12V to 3.3V in their project, but they failed the radiation spurious test in the FCC certification test of BT.
The reason for asking us about this question is because…
Part Number: LP2950 Hi,
the datasheet of LP2950 mentions in chapter 7.1 that it features a Thermal Shutdown. How does it work? At what temperature does it switch of the device? Is it available also in the fixed voltage version of the device?
Thanks…
Part Number: LP2950 Hi sir/madam,
I am confused that datasheet of LP2950 denoted the temperature 0~0℃ (red line in the following image) , I want to know what does it mean? Could you enlighten me on it? Thanks.
Regards,
Jenny
Hi Jason,
Thank your for your reply.
I'm sorry for late reply, I had a new year holidays.
I understand LP2950 has a internal parastic diode and need to implement external shottkey diode.
I'll share this information with the customer.
Best…
Other Parts Discussed in Thread: LP2950 Hi, team,
Now we have one question about LP2950 from Customer. They are now using it for 10 bit ADC with 1% resistor divider. When doing the -25 degree low temperature test, the maximum output change of LP2950…
Other Parts Discussed in Thread: LP2950 Hello,
I'm attempting to use the 12V output of a LM340T (12V LDO) as the input for a LP2950 (5V LDO). Both have decoupling capacitor values as per datasheet recommendation, and they are being connected through…
Hi,
I need to confirm the operating temperature of LP2950-50LPRE3.
When I check the TI web ( http://www.ti.com/product/lp2950-50 ) or the datasheet ( http://www.ti.com/lit/ds/symlink/lp2950-50.pdf , 19 page) shows the Operating temp is 0 to 0.
I…