Part Number: LP2951 Other Parts Discussed in Thread: TLV709 , TLV760 Hi team,
Could you please recommend a device with below spec requirement?
Vinmax>25V
Vout=15V
Iout>=100mA
enable
low cost
Part Number: LP2951 Other Parts Discussed in Thread: LP2950-N Hi team,
My customer is currently using LP2951ACMM-3.3/NOPB but is having sourcing issues, LP2951CMM-3.3/NOPB seems like a good replacement but I didn't find the description on the difference…
Part Number: LP2951 HI
LP2951 is our 15V to 5V regulator IC. 5V is going into the digital Isolator IC ISO7220ADRG4. The digital isolator is supplying PWM pulses to LLC driver UCC27714DR which is driving LLC mosfets. whenever LLC mosfets got shorted or…
Part Number: LP2951 Other Parts Discussed in Thread: TPS746 , TPS7A49 , Hi Team, seeking for some support.
Like to provide bypassing between the IN and OUT of LDOs. I am considering LP2951 LP38502 TPS746 TPS7A49 and/or TLV766, but I imagine the answer is…
Part Number: LP2951 hi teams:
1. U1 :LP2951-DR.
2. input :12V ,OUT 5V 0.03A.
3. The output voltage of 3PCS is very small, almost zero . Please help review schematic diagram.
Part Number: LP2951 Hello,
are you able to clarify what the ">" in the marking callout would mean? Is this a variable callout of the last digit that can be anything less than D?
ti.com/lit/ds/symlink/lp2950-n.pdf?HQS=dis-dk-null-digikeymode…
Part Number: LP2951 1. Can the fixed output versions LP2951-30, LP2951-33, LP2951-50 be connected with external feedback resistors to output adjustable voltage?
2. If LP2951-33 can also output adjustable voltage, what is the difference between LP2951…
Part Number: LP2951 Hi, we are using LP2951CM/NOPB in one of our designs and this part isn't currently available/has a long lead time.
We are using the part in a current source configuration, see attached diagram of our circuit and the image from…