Part Number: LP2951-N Hello,
We are using the LP2951ACMMX-3.3/NOPB component and would like to test the undervoltage threshold. The test circuit is shown below. We power on both 5VD_safe and 3.3V_PSU at the same time. We expect the LDO to output 3.3V…
Part Number: LP2951-N Tool/software: In our application using LP2951CSD/NOPB, we've found that if the current limit is in the lower range of the allowable limit, the output can get stuck at power on, due to a heavy load on the output.
In the datasheet…
Part Number: LP2951-N Tool/software: Part: LP2951CMX/NOPB
What is the best practice for increasing the ESR of output capacitors in LDOs?
Often, multiple output capacitors are used in parallel because each chip that requires the LDO's output voltage…
Part Number: LP2951-N Want to use LP5951-N's under voltage function
refer to the datasheet below
If use 3.3V version, then the under voltage minimum is 3.254V *95% or 3.3V*95%?
Part Number: LP2951-N Other Parts Discussed in Thread: TIDA-010015 Hello Sir/Ma'am,
I want to simulate the schematics of TIDA-010015(480W SMPS) design in SIMetrix software. But for this I have to use the SIMPLIS model of LP2951-N. But unfortunately…
Part Number: LP2951-N Hello ,
Is LP2951ACMX/NOPB same as LP2951-N right?
As per datasheet,
We have two statements for shutdown pin connection which is present:
1. Here it says if shutdown pin is low , it turns off the regulator.
2. Here…
Nick Butts said: but if it was put into current limit for hours (I think you were just making a point and not suggesting that it is this) this could be a concern
Correct. At the moment, there is just nothing preventing that from happening.
Nick…
Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 I would like to operate the LP2951ACSD/NOPB in an environment where Ta=125C, input voltage of 10-30Vdc, output voltage set to 10V using 732K between Vout and FB pin and 100K between FB pin…