Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 When pulling the LP2951 shutdown pin low to disable the regulator, we noticed that the error (open collector output) pin is being pulled low. Does the error detection comparator circuit stay…
Part Number: LP2951-N Team,
my customer is using LP2951ACMM-3.3. Nominal Vin is 10V.
As part of failure considerations, they would like to know the behavior of the device when abs max Vin is exceeded -> Vin =38V It's ok for the device to be destroyed…
Part Number: LP2951-N Other Parts Discussed in Thread: TINA-TI , LP2951 , LP38798 , Tool/software: TINA-TI or Spice Models Hi, I'm doing some simulation using TINA with the LP2951-N3P3. I noticed that when SHUTDOWN is asserted the output capacitor is rapidly…
Hi Ian,
LP2951-N was originally released by National Semiconductor before TI acquired the company. The LP2951 is the version of the device that was released by TI while the two companies were competitors.
Very Respectfully,
Ryan
Part Number: LP2951-N Hi
LP2951ACSDX/NOPB is this the right part for the 5V fixed output voltage in WSON Package? if not please suggest, I am looking for LP2951-N in WSON 5V fixed output voltage.
Best Regards
Umesh Thapa
Part Number: SN6505D-Q1 Other Parts Discussed in Thread: SN6505B , LP2951-Q1 , TL431-Q1 Hello,
I need some information related to a family of SN6505B/D push-pull drivers.
Please, attached is a draft schematic.
The characteristics of the circuit are:
SN6505B…
Part Number: LP2951-N Hi,
We have design needs very accurate output. So, we are taking the full equation Vout = Vref * (1 + R1/R2) + IFB*R1. For IFB*R1, should this portion be negative? Means need to minus of IFB*R1?
Thanks.
- YY
Part Number: LP2951-N Other Parts Discussed in Thread: LP2951 HI ALL
I need an answer for the below query.
I am using LP2951 adjustable LDO for my oscillator Circuit which draws 10mA to 15mA of current. I have used 0.47UF tantalum capacitor at the output…
Part Number: LP2951-N Hi.
I have a question regarding the output capacitors connected to a LP2951-N, where the datasheet have different statements:
Paragraph 8.3.7 (page 17) says, that the output capacitor can be a ceramic type with a ESR down to 6 …