Part Number: LP2951 Other Parts Discussed in Thread: LP2954 Dear E2E,
Please help to propose a p2p solution with LP2951-50DR, but Iout capability needs to be higher than 100mA.
BR,
Andy
Hi Bala,
The LP2954 has similar thermal performance to the LP3856-ADJ in the TO-263 and TO-220 packages. From the datasheet, θjc(bot) is 1.0 C/W and typical θch values will depend on the interface material:
The heat sink will need a θha such…
Hi Craig,
we have many catalog parts comparable to TL75L1 and have higher output current such as LP2960, LP2954, LP2954A, LP2952N, and LP 2953
BR,
Haidar
Hello Wilson,
Do you need an exact pin to pin replacement? Or just any SOIC is fine?
The LM317L (need to go with I version of the device for full temperature range) is the cheapest solution for a replacement, but isn't 14 pin SOIC.
If you mean…
Using the LP2954IMX adjustable version in SO8 for adjustable voltage output as in Figure 24 in the data sheet.
For 5 VDC output operation, the SENSE and 5V TAP pins are called out in the data sheet as being:
"pin-strapped for 5V operation using its internal…