Part Number: LP2954A can i get some clarification on the statement in the datesheet that states the following
" The regulator output can be left connected to an active voltage source (such as a battery) with the regulator input power turned off, as…
Part Number: LP2954A I found an encoded PCSPICE model of the LP2954A, but this is useless for the TINA-simulator. Is it possible to create the TINA-model?
Other Parts Discussed in Thread: LP2954 The datasheet of LP2954 indicate that the RTHja is 44.3°C/W but I don't the size of the copper pad. Can somebody tell me the recommended footprint and the value of RTHja associated.
Thanks.
Part Number: LP2954A The datasheet states that the output voltage can be programmed from 1.23 to 29 volts. In section 7.3.3 (Output Isolation) the following is stated: "T he regulator output can be left connected to an active voltage source (such as a…
Part Number: LP2954A Other Parts Discussed in Thread: LP2954 , TPS7B86-Q1 , LM5069 Dear Power Management Team,
I have some questions about the output Isolation feature et some charateristics of the LP2954 :
- Is the output stage a bipolar transistor…
Hi Jim,
I've noted the model request for future development, but can't make any specific guarantees about if/when this would be available for now.
If customers are ok with not being able to access the REF, COMP_INPUT, and COMP_OUTPUT pins then the…
Hi Craig,
we have many catalog parts comparable to TL75L1 and have higher output current such as LP2960, LP2954, LP2954A, LP2952N, and LP 2953
BR,
Haidar