Hi Henrik,
There are a couple potential fixes for this. It looks like the source of the BSS139 is not able to rise high enough to pass UVLO on the LP2980. To fix this, the gate needs to be biased higher to allow the source to rise enough to properly…
Part Number: LP2980-N We have been using the LP2980IM533 for 15 years. However, it appears that the latest design revision has different output capacitor ESR requirements compared to the Legacy chip.
The legacy chip ESR is 20m ohm to 20 ohm. The new…
Part Number: LP2980-N Customer says part number LP2980IM5-5.0/NOPB is defective. Below is what they said.
Digi-Key Part Number LP2980IM5-5.0/NOPBDKR-ND Internal Part Number 1100-10002674 Quantity Affected 500pcs Who should we contact for additional…
Part Number: LP2980-N US COD material (qty:11408pcs ) is currently failing our ICT testing, we would like to arrange a return for this batch and have it replaced with material with COD UK instead.
TI has requested to fill in CPR form
Part Number: LP2980-N We are using LP2980IM5-3.3/NOPB to generate 3.3 V supply for an encoder IC.
Observation:
With 1uF MLCC output capacitor, we observe
60mVpp ripple on LDO output
Ripple has a sawtooth-like waveform
Issue becomes more pronounced…
Part Number: LP2980-N Tool/software: Hi TI Team,
Could you please confirm the LP2980AIM5-5.0/NOPB whether the method we used is correct or do they have any suggestions?
The following information is for your reference.
Product: 9021545,
Defect…
Part Number: LP2980-N Test Abnormal Phenomenon
The current ICT test limits are defined based on KGB measured values. The KGB test value is 3.3V, and the upper and lower limits are set to ±5% (Jabil development team specification).
During testing…
Part Number: LP2980-N Hi team,
May I know how could customer identify LP2980-N old chip vs new chip?
From which DC, the chip are new chip? Thank you!
Best regards
Yunjing
Part Number: LP2980-N
Asper data sheet there is difference in chip component mentioned as legacy chip and new chip and showing lot of difference in data sheet.
Need to understand the lots sented to us is legacy chip or new chip.
Part Number: LP2980-N Tool/software: We are facing an issue with LP2980AIM5X-5.0/N0PB .
Based on the shipping label, the component is from CSO: RFB (new chip) and is made with post-PCN material (PCN# 20230906001.1A).
During ICT testing, we observed…