Part Number: LP2985 Other Parts Discussed in Thread: TPS763 Hello,
My customer is trying to drop LP2985-50DBVR into their existing schematic below with no board changes because of supply issues with TPS763.
Specs:
Vin can be as low as 6.4V.
We planned…
Part Number: LP2985
Hi Experts,
Good day. We would like to ask the theta JC information of the following orderable part in DBV-5P package:
LP2985-50DBVR
Such information is not available from its D/S. Can you provide it?
Thank you for your support…
Part Number: LP2985 Hi team,
In the original thread here , I saw LP2985A doesn't support Enable.
Does Enable mean the ‘ON/OFF’ operation? If yes, from the datasheet, i think LP2986A can support Enable. Could you please help with the question…
Part Number: LP2985 Hi,
We are developing a device using your component LP2985IM5-1.8/NOPB which is considered as a critical component for our device according to the ISO 13485 standard.
Can you send us the proof of certifications announced in the data…
Part Number: LP2985 Customer verify the Thermal parameter and n eed the data of "power dissipation & θJC" for LP2985 .
Datasheet have no data could reference.
Part Number: LP2985 hi Team,
I'd like to ask for your help about LP2985-33 OCP and OTP details:
1. what's the set point for OCP and OTP?
2. does there any hysteresis for OCP and OTP?
3. what's the accuracy for OCP and OTP?
Thanks.
Part Number: LP2985 Hello, the LP 2985 small package places a limit on heat dissipation. With a 12V input voltage and a 40mA (280mW) current draw what would be the approximate case temperature assuming an ambient temperature of 25c
Part Number: LP2985-N We are confirming that ESR of output capacitor is in stable region described in Figure 22.
We assume that frequency value of ESR is 1MHz by referring to 8.2.1 Design Requirements Table 1 Input Voltage. Is this frequency condition…