Part Number: LP2998
Pleas help confirm below shipment if the actual part receive is correct. Parts is currently hold at our receiving. Appreciate you immediate response.
PO and Packing List- MPN LP2998MRX/ N OPB vs Actual Label-Rec'd MPN:LP2998MRX…
Part Number: LP2998 Tool/software: Hello
We are using the LP2998MR in a supercapacitor balancing application (2 × 3.3 F, 2.7 V supercaps ). Part of the circuit is based on TI reference design https://www.ti.com/tool/PMP9766#tech-docs
The boards are…
Part Number: LP2998 Tool/software: Hi team,
According to the attached E2E forum, for LP2998MRX/NOPB, only the DDA008A package is currently being produced among DDA008A, DDA008B, and DDA008D. Is it the same for LP2998MR/NOPB — is it also only available…
Part Number: LP2998 Hi We are using LP2998 in our desing. Please refer below schematic. When measured the input is 1.807V but the out put at the VREF is only 0.857V. Can you please verify and hlep us to resolve the issue. Regards, Raju
Part Number: LP2998 Other Parts Discussed in Thread: LM2831 Hi,
We have used LP2998MR for DDR3 termination whose inputs are 1.5V for PVIN and VDDQ, 3.3V for AVIN. Could you please review the attached schematics? Also, I need to know what is required…
Part Number: LP2998 Tool/software: Dear TI Engineer,
Can you help to review the design of LP2998? The schematic is as below:
We have doubts about the level of the /SD pin, when we pull down this pin, there will be no output from the VTT pin, but…
Part Number: LP2998 Hi,
Is it OK to float the LP2998MR (SO PowerPAD) Thermal Pad?
We are considering replacing from the LP2996M/NOPB. Since we have the LP2998MR(SO PowerPAD) in our company, I would like to know if we can replace it without using Thermal…
Part Number: LP2998 Hello,
There are three package outline figures, DDA008A, DDA008B, and DDA008D on its datasheet.
Can you explain the differences among them.
We would like to know the package outline of LP2998MRX/NOPB.
Thank you
Part Number: LP2998 I am looking for the following parameters and I don’t see them in the datasheet. Can you please help me with them?
Part number: LP2998MR
Here are the values I am looking for:
Rated pin current
Rated operating frequency
…