Part Number: LP2998-Q1 Other Parts Discussed in Thread: TPS51200A-Q1 , Hello,
The part TPS51200A-Q1 is not available for procurement.
Could you pls suggest an alternate part. we have used in our proto design..but now we are going for production..but…
Part Number: LP2998 Other Parts Discussed in Thread: TPS51200
Hi Team,
I would like to use LP2998 in the following configuration.
AVIN,PDIN,VDDQ=3.3V, VTT=1.65V output
Is it possible?
Best Regards, Tom
Part Number: LP2998-Q1 Hi Team,
Our customer wants to use LP2998-1 for DDR3L. The input voltage of DDR3L is 1.35V, and our minimum input voltage VDDQ is 1.35V. Can it work normal at all condition?( customer is worried about it)
Thanks.
Part Number: LP2998-Q1 Other Parts Discussed in Thread: LP2998EVAL , Hi team,
Hope you‘re doing well!
1、What is the delay/calculation between VTT and VDDQ?
2、Can VDDQ be connected to PWM to dynamically adjust the output of VTT?
3、How will VTT…
Part Number: LP2998 Hello,
At our project we need to supply VREF for DDR3 reference pin, and also to the MCU DDR_VREF pin.
The DDR_VREF pin current consumption can be at the maximum state 1mA.
1. Can the LP2998 VREF output supply this amount…
Part Number: LP2998 Hi Team,
Could you please review the attached design using LP2998MA/NOPB.
Please let me know your comments.
Thank you.
Regards,
Marvin
Part Number: LP2998
Hi Team, using LP2998 in my design for DDR3 Termination voltage generation For DDR3(4Gb*2), will it support current range.
we want to connect AVIN =3.3V and PVIN=VDDQ=1.5V.
Thank you.
-Mark
Part Number: LP2998 For example datasheet figure 26 and 27, unused VREF condition.
Is VREF pin OK to left floating on unused condition?
Best regards,
Satoshi
Part Number: LP2998
Hello Team,
What is the value of required continuous output current for DDR3L termination?
The datasheet shows that it is tested at ±0.5A, so is this the required value?
Other application notes mentioned 1.5A for DDR1 and 0…