Part Number: LP2998-Q1 HI,
I received the following question from my customer.
Could you tell me the absolute maximum ratings of source/sink current values if these exist?
We are recognizing that these are not mentioned on the datasheet.
Best Regards…
Other Parts Discussed in Thread: LP2998-Q1 Our customer consider to use LP2998-Q1 at DDR3 application.
They would like to know Supply current of this part at DDR3 application .
I found " IQ","ISD","IQ_SD","Iv" PARAMETER…
Other Parts Discussed in Thread: LP2998-Q1 Dear all,
I would like to know how to calculate theta-ja.
Is there formula to calculate theta-ja according to different situation?
Best regards,
Other Parts Discussed in Thread: TPS51200-Q1 , TPS51200 Hi
Does this device has current limit protection?
The output current depends on PVIN as mentioned at datasheet.
The output current are limited within 0.5A?0.4A? for DDR3 when the PVIN=VDDQ=1.5V and…
Other Parts Discussed in Thread: LP2998 Please tell me shutdown current of LP2998 at "AVIN=3.3V PVIN=VDDQ=1.5V SD=0V".
Is the electric current flowing through AVIN VDDQ and PVIN pin several amperes at "AVIN=3.3V PVIN=VDDQ=1.5V SD=0V"?…
Other Parts Discussed in Thread: LP2998 , TPS51200 , TPS53317A , TPS51200-Q1 The LP2998 datasheet says, "The device also supports DDR3 and DDR3L VTT bus termination with VDDQ min of 1.35 V". This could be interpreted to mean that at 1.34999V the…