As per the orange trace (VOUT at 2V/div), you seem to be getting 3.3V at the output. Could you show me where you are seeing 4.8V on the output or if I am reading something incorrectly from the scopeshot above?
Part Number: LP38512-ADJ Other Parts Discussed in Thread: TPS7A52 , TPS74801 Hello,
I cannot find the LP38512-ADJ model in PSPICE for TI (just installed the latest version), also the web page doesn't list any option to get a simulation model.
LP38512…
Part Number: LP38512-ADJ Other Parts Discussed in Thread: TPS7A7001 , TPS7A57 Hi,
We configured this LDO as shown in the Typical Application circuit diagram.
Vin = 5V
Vout = 3.3V typical
Maximum load current 500mA
R1 (feedback) = Trimmer Resistor (3296W…
Part Number: LP38512-ADJ Other Parts Discussed in Thread: LP38512 Hello support team,
My customer plan to use LP38512MR-ADJ and ask some questions, could you support?
Usage setup: VIN: 3.7V, VOUT: 3.0V
*What is maximum output capacitance? They plan to…
Part Number: LP38512-ADJ Hi Team,
Would please help to confirm junction to ambient thermal resistor of LP38512-ADJ(SO PowerPad)? It's 168W/C in the datasheet, seems to be so large. The test results show it should be around 40W/C per customer's feedback…
Part Number: LP38512-ADJ Hi Experts,
Good day.
I am not sure if my understanding is correct with the LP38512-ADJ.
If I wanted to provide the lowest possible output of the subjected LDO, Vout = 500mV, based from page 10 of its datasheet guidance formula…
Part Number: LP38512 Hi Sir,
Pls kindly reference as below customer schematic.
O/P will have 6ms delay after EN, what will possible cause it?
Thanks, Ian.
Part Number: LP38512 Our Customer has query on LP38512
td(ON-Delay) value mentioned in Electrical char and the one which is shown in the subsequent plot are different values. They would like to understand what are the max and min values for td(ON-delay…
Part Number: LP38512-ADJ Other Parts Discussed in Thread: LP38512 , Hi Team,
Our customer is using LP38512-ADJ for 3.3V to 1.8V application for DLP DMD power supply, but recently they found there is about 1 in 10000 probability for LP38512 no 1.8V output…