Hi Jim,
I followed your instructions but, unfortunately, still no success. After starting an acquisition Wavevision produces the same error message as before: "Board failed to collect samples...". However, I think I can confirm that wavevision indeed…
Colin,
I do not know of a linear regulator with a vref of 0.4V, however, we do have several with a vref of 0.5V.
These would include the LP5922, TPS7A7001, LP38512, LP38513, and TPS7A7002.
I will move your posting to the Linear regulator group to…
Other Parts Discussed in Thread: ADC10D1500 , LM25576 , LP38513 I am working in a board with a ADC10D1500 and the supply is designed based on "ADC0xD1520RB Reference Board".
THE ADC requires 1.9V that are generated from a 12V voltage supply. In a first…
Hello Bridget,
The 6th pin of LP38513-ADJ is the ground pad located on the bottom side of the device.
The voltages you are seeing on those pins are not correct however and imply that the input voltage to the device (Pin2) is too low.
Here are what…
Hi Sir,
Can i use LP38513-adj to generate 3.3V and 1.2V? Can i add the 8 x 10 uf capacitor in the output bus (decoupling) using this regulator. please let me know.
Thanks,
V. Prakash
Feiran,
looking at the ADC07D1520 EVM schematic, I noticed the FMC pins have connection made on rows besides H, G, D, and C. Therefore, this is HPC connection
reference:
ADC0xD1520RB_R1_Schematic_07-27-2K12.pdf
-Kang
Hi Alex,
I think I have found what the issue may be - I believe the files are outdated. Please try with the below file.
3771.ADC12D1X00RF_RB-SCH_B.pdf
Thanks, Chase
Part Number: ADC12D1600RFRB Hi Experts,
I setup WAVEVISION 5 and drivers for Win10, and power up ADC12D1600RFRB with 12Vin from power supply.
but WAVEVISION 5 does not capture any hardware device after EVM power up.
The attached files are what I…