Part Number: LP3856-ADJ Tool/software: Hello,
We currently have a design in which we unintentionally have power being fed back into the Vout port of the device. The voltage being read at the terminal is -0.54V when the 6.4V rail is powered off. The specifications…
Part Number: LP3856-ADJ Other Parts Discussed in Thread: LP3856
Hi,
I have been using LP3856 for one of my circuit. But I found the output voltage is not stable. It keeps on increasing.
Here are my parameters:
Input voltage - 5.41 V
Output voltage - 5…
Part Number: LP3856 Other Parts Discussed in Thread: TPS7A53 , TPS7A54 Hi,
Good Day.
If LP3856ES-2.5/NOPB (2.5V/3A) recommended for Voltage rail to an FPGA device?
Please advise. Thank you very much.
Best Regards,
Ray Vincent
Part Number: LP3856-ADJ Hello I use this component in a multi-power supply.
During the final test of the output voltage, I found that the deviations are greater than indicated in the data sheet.
Here are the results:
Here are the drawing of the 5V-output…
Part Number: LP3856
I'm trying to better understand the description here.
Is it safe to directly tie the /SD pin to VIN if shutdown functionality is unused?
Or do I still need to pull up through a 10kOhm resistor?
Part Number: LP3856 Other Parts Discussed in Thread: , LP2954 Hi,
I'm planning to use LP3856 in one of my design. Here is the requirement,
1)Vout= 2.4V to 6.0V
2)Iout= up to 2A., typ (1.75A)
3) LDO output should be programmable through serial interface…
Part Number: LP3853 Other Parts Discussed in Thread: LP3856 , Hello,
The current product uses TPS75825KTT, but since it is difficult to obtain, I'm thinking of replacing it with LP3853ESX-2.5.
I am using EN of TPS75825KTT, but 5pin is not connected…
Other Parts Discussed in Thread: LP3856 Dear Sir,
I am going to calculate the theaml of TO-256 package of LM3896 but there is no record of θJc in the specification. May you give me more details paramater for reference, Thansk.
Other Parts Discussed in Thread: LP3856 I need to use the scheme with LP3856: Input voltage is 6.5 V. The output voltage is 4.5 V. It is possible to translate in Shutdown mode using a microcontroller, which is powered by a 3 V. Are there any features of…
Other Parts Discussed in Thread: LP3856 Hi TIer
I have experienced VIN drop when I control SD pin low to high.
Output current is only around 3mA.
Who can explain why it is occurred?