Part Number: LP38691-ADJ Other Parts Discussed in Thread: TLV767 , LMG1020 , TPS7A90 I would like to use LP3869x- ADJ for Vout =5V.
The load transient waveform that is being provided in datasheet is for Vout = 1.25 V, I would be thankful if you could provide…
Part Number: TPS7B4254-Q1 Hello E2E team,
Referring to section 6.1, footnote 4 specs of the device datasheet, "When the (ADJ – IN) voltage is higher than 18 V, the (ADJ – OUT) voltage should be maintained lower than 18 V, otherwise the device can be damaged…
Hi Tomasz,
Thanks for the clarification and taking the time to explain!
About the tracking LDO -- While the tracking LDO does offer excellent accuracy, this isn't Vout accuracy in the same sense you'd think of a traditional LDO. The accuracy is tracking…
Part Number: LP38691-ADJ Other Parts Discussed in Thread: LP38691 , Hello,
I've see your answer to previous similar question, but I was too busy to answer you..
Neitheless I found differents working of the same component on the same board !!!
On the…
Thanks for your reply Frank,
We are currently using the LM5360x-RB (Automotive grade) 36-V Synchronous, 2.1-MHz, Automotive Step-Down DC-DC Converter. Kindly consider the voltage rating of the same LM5360x-Q1 and package we use is WSON-10. We had received…
Part Number: LP38691-ADJ Hello,
I have a serious problem with limitation current of the device.
On an actual PCB we use LP39681-adj LDO regulators, and I have problem with them...
Current limiting doesn't work anyway, if I short output or if I connect…
Hi Anthony,
No, it is not possible to dynamically adj the output voltage via a current DAC. The FB pin of the TPS54361-Q1 is a high impedance input with no internal resistors connected to the output.
Ben
Part Number: LM53600-Q1 I would like to use the LM53601-Q1-ADJ to produce 3.0V from an input voltage of Vin = 12V +/-15% (10.2 < Vin < 13.8 V). The desired output voltage is slightly below the recommended operating conditions given in Section 7…