Hi Anthony,
No, it is not possible to dynamically adj the output voltage via a current DAC. The FB pin of the TPS54361-Q1 is a high impedance input with no internal resistors connected to the output.
Ben
Part Number: LM53600-Q1 I would like to use the LM53601-Q1-ADJ to produce 3.0V from an input voltage of Vin = 12V +/-15% (10.2 < Vin < 13.8 V). The desired output voltage is slightly below the recommended operating conditions given in Section 7…
Part Number: TPS7B4254-Q1 Hi Team
we will use LM4050-5.0-Q1(5V Shunt Voltage Reference) for powering ADJ pin of TPS7B4254-Q1.
we would like to minimize current consumption at LM4050-5.0-Q1.
may I ask how much the leakage sink current into ADJ pin is if…
Part Number: TPS7B4253-Q1 Hi Team,
I noticed in the TPS7B4253-Q1 datasheet that there are two different packages, one that has an enable pin (HTSSOP) and the other only has a adjust pin (DDA). For the HTSSOP package offering with the enable pin, it say…
Other Parts Discussed in Thread: TPS784 240130_TI_Production Location.xlsx
Hi,
I am interested in gathering information about production location for power supply parts.
Please find the attached sheet with required details.
Best Regards
Pawel Szkolik …
Part Number: TPS65150-Q1 Hi Team,
I have customer using TPS65150-Q1, but the voltage gate shaping function is not required, thus the CTRL pin is connecting to VIN as always high. In this user case, what's shall we do with ADJ pin ? Could it be left…
Part Number: TPS7B4254-Q1 Team,
IN is battery at 12V and ADJ is currently low. What is the timing from ADJ considered to be high (>=2V per the test parameters in Electrical Characteristics ) to OUT of the LDO ramping and tracking ADJ?
Part Number: LP38691-Q1 Other Parts Discussed in Thread: LP38691 Hello,
Datasheet has following explanation about reverse current.
“The current in the parasitic diode must be limited to less than 1-A continuous and 5-A peak.”
Please advise…
Part Number: TPS65150-Q1 hello
Input voltage=5V,
Output Max Value: AVDD=13V/150mA,VGH= 20V/20mA,VGL -10V/20mA
what is the Absolute Maximum Rating of Voltage on these pins, COMP, ADJ, DLY1, DLY2, FDLY?
we want to choose the Lowest Voltage Rating capacitances…