Part Number: LM135 Other Parts Discussed in Thread: LM95172-Q1 Hello,
I'm using a temperature sensor LM135AH for a wide-temperature measurements ranging from 25°C - 175°C. I'm attaching the schematic below, In previous designs, I used the 5V rail and…
Hello,
Please answer following question from customer.
Input voltage absolute maximum ratings is 12V max.
Please advise what will happen when 16V is applied to IN terminal.
For example device will be damaged but smoke, burn and IN-OUT short will not…
Part Number: LMQ66410-Q1 Other Parts Discussed in Thread: LMQ66430 Hello Dear TI Team,
Regarding the LMQ66410-Q1 device, according to its Data Sheet, SNVSC78B – FEBRUARY 2022 – REVISED MAY 2023, 5 Device Comparison Table on Page 3,
there is…
Other Parts Discussed in Thread: LP38691 , TINA-TI , LP38691-Q1 Hello,
Please advise how to use “LP38691_3P3 PSpice Transient Model” on the following page on TINA-TI, or give me TINA-TI model.
www.ti.com/.../toolssoftware
Best Regards.
Other Parts Discussed in Thread: LM53601-Q1 , LM43601 Hi~ All..
Customer want to use spread spectrum function, so we suggested LM53601-Q1 in automotive application.
But in datasheet, LM53601-Q1 only can support down to 3.3V, but there is description that…
Other Parts Discussed in Thread: TPS7B4253-Q1 For applications that use TPS7B4253-Q1 to power external sensors, the following circuit is used. When software-controlled EN/ADJ switches between activation and non-activation, it is found that the output …
Hey Adrian,
This does not seem like a stability issue because the part is not oscillating.
This might be caused by the internal soft-start circuitry. The part could be starting up faster than the internal circuitry allows.
After speaking with colleagues…
Part Number: TPS3704 Hello team,
For our project we want to monitor the output voltages of a PMIC (LP7745-Q1).
We are looking into the supply voltage supervisor: TPS37044,. We would like to calculate the accuracy of the device for 4 different rails 1V…
Part Number: LM21215A Other Parts Discussed in Thread: TPS62873-Q1 Dears:
when input=3.3V, output use DAC to do ADJ, customer found that LM21215A work frequency will change to 250KHz and output voltage ripple will up to 50mV.
we tried to remove capacitor…