Part Number: LP38692-ADJ Hi Team,
We are using the LP38692SD-ADJ/NOPB LDO part in our schematics. We are using the same part in couple of instances, I had attached the schematic Images below, Kindly review the schematics and share your valuable feedback…
Part Number: LP38692 Hi expert,
Customer has two questions:
1. What is the Dropout voltage (Vdo) (Typ) (mV) 250 test condition?
2. When Input id 5.5V, output voltage is 5V, and current is 0.5A, what is the typical and max dropout voltage?
Part Number: LP38692 Other Parts Discussed in Thread: TPS709 , LP38690 The LP38692 will be used to provide Vdd to my system including the microcontroller (MCU).
The MCU will have a GPIO, configured as output, connected to the EN pin of the 38692 to…
Part Number: LP38692 I have a request. I want the reliability data of LP38692MP-2.5 / NOPB. There was no information on the TI website.
www.ti.com/.../home
Will you provide it?
best regards.
Part Number: LP38692 I am using the LP38692 for regulating the voltage from 9V to 5V.....
Could you please suggest me the quantitative procedure for the selection of the output and input capacitors......
Part Number: LP38692-ADJ Other Parts Discussed in Thread: LP38693-ADJEV Hi Team
. Could you send me Gerbers and schematic for AN-1757 LP38693SD-ADJ Evaluation Board please, because they are missing from your webpage?
Part Number: LP38692 Hi all Would you mind if we ask LP38692? How much is VEN's Absolute Maximum Ratings? We assume that VEN must be less than VIN. Because of internal diode between VIN and VEN, in case of VEN > VIN, it might flow the the current into…
Part Number: LP38692 Hi,
I have used LP38692SD-ADJ/NOPB in one of my board which can take Vin up to 10V and i am generating 3.3V, for some reasons after testing my boards we need to generate 3.3V from 12V which will call for board respin.
I am thinking…
Part Number: LP38692 Other Parts Discussed in Thread: TPS7A45 Hi,
I have used LP38692SD-ADJ/NOPB in one of my board but now i want to use a LDO which can source output current greater than 1.2 Amp and voltage 5V with input 6V and should be footprint…