Part Number: LP5012 Other Parts Discussed in Thread: LP5036
Tool/software:
I have two LP5012 devices on a custom board connected to a nRF52840. Only the right one powers the four LEDs it's connected to but both seem to respond to I2C commands just…
Part Number: LP5012 Tool/software: Hello,
We are currently using your LP5012 driver on our devices which so far have always worked well. However, we found ourselves in the situation of having to use 4 LP5012 drivers on the same I2C communication line…
Part Number: LP5012 Tool/software: According to the request of the client, we need to provide FDM (Full Material Disclosure) information of the following materials. Please assist in processing this matter.
TPS25200DRVR
INA231AIYFFR
…
Part Number: LP5012 Tool/software: I would like to connect the LP5012 to an I3C bus. Question is if the digital interface logic includes a 50ns glitch filter? Kind Regards, Ben
Part Number: LP5012 Other Parts Discussed in Thread: LP5036 , , LP5030 , LP5018 , LP5024 , LP5009 Tool/software: Good day, colleagues,
My customer is currently using 4 pieces of the LP5036 LED driver in a project and would like to add one LP5012 to…
Part Number: LP5012 Other Parts Discussed in Thread: UCC27517A Tool/software: Im a software guy, who knows little bit of electronics... i want to use the LP5012 to drive 12V RGB LED Strips
the led output is duped for out1 and out2 of course to get RGB…
Part Number: LP5012 Tool/software: Hello,
im working on an IOT device that combine an MCU and a LP5012 LED driver.
my purpose is to run an LED driver on a constant current of 20 mA
i have create the following circuit using LP 5012
when trying…
Part Number: LP5012 Tool/software: Hi team,
Can LP5012 turn on multi LEDs simultaneously? Customer tried it but couldn't it.
Is this due to of Phase-Shifting function? Best regards, Goto
Part Number: LP5012 Hello
I just want to confirm this is acceptable and correct:
Going to use LP5012 in a design where the I2C is shared between different slaves ( addr. is different ), the pull up resistors for SCL and SDA is connected to 3.3V…