Hi, guy,
Reference to page 5 of the datasheet(which is attached following), the LP5012 is designed with dependent color mixing and intensity control. you can control the LED brightness separably for each LED by the color-mixing.
The PWM signal is…
Part Number: LP5012 1、In page33 , the EN is connected to MCU's GPIO. Now I want to connect it to the VIN. It can be connected to the power VIN directly, right? 2、Is there any Rpullup or Rpulldown inside the IC LP5012?
Part Number: LP5012 Other Parts Discussed in Thread: LP5569 Hi, Team
Our customer using both LP5012 and LP5569 in their smart speaker. they needs to check whether these two devices will reset register to default value when pull the EN pin to Low. I…
Part Number: LP5012 Hello Guys,
Good day.
Our customer is currently facing some issues with the LP5012 chip. He is facing some difficulties interfacing with this IC despite using the datasheet extensively. He is unable to sink the current entirely…
Part Number: LP5012 Hello E2E Team,
We are considering the LP5012 LED driver for a new design but we have a concern that the pulsed nature of the light output may possible cause us problems, so we're looking for a backup plan to mitigate the risk. …
Part Number: LP5012 Other Parts Discussed in Thread: TLC5940-EP , LP5569 , Hi Team,
Can you please check and advise with following request possible solution or alternative device?
"
When the LP5012RUKR manufacturer code product is powered and at…
Part Number: LP5012 Hello,
Our customer has a question if EN, SCL, SDA can support 1.8V logic input level without a level shifter. Even though I can see 0.4V VIL, 1.4V VIH in the datasheet, could you confirm if LP5012 can support 1.8V logic iput without…
Part Number: LP5012
Hello Team,
can you confirm the following options of using the output drivers?
They both look good, while the last point is a "misuse" it is reasonable to save space and cost.
1. It should be possible to operate the LEDs mixed…
Part Number: LP5012 Hi support team,
LP5012RUKR is used by incorporating it in the sub board. If the power supply is stopped due to poor contact with the main board, I think that communication will not resume unless it is restored by the sequence shown…
Part Number: LP5012 Hello lovely people,
I have an LP5012 on my PCB (attached layout), and I'm having an issue with getting the LEDs to light. I can confirm I can write/read-back registers.
I'm also wondering, when I power on the PCB I can read…