Part Number: LP5018 Hi Team,
My customer measured the SCL low period time is only 1.26us which is less than SPEC 1.3us. Will have any concern for this one? Can we use standard to measure it?
Note. The concern is from due our device VIH and VIL definition…
Part Number: LP5018 Hello,
I'm slightly confused on the channel to channel current error spec. The datasheet describes it as +/-7%, but based on the provided equation it seems like the difference between out1 and out2 could be 14%:
If I have…
Part Number: LP5018 Other Parts Discussed in Thread: TLC59116F , , TLC59116 Hi team,
I am looking for a device similar to LP5018 but with a Vout at least 12V. I am looking at TLC59116F as it looks at least kind of similar, but I wanted to see if there…
Part Number: LP5018 Other Parts Discussed in Thread: LP5569 Hi Team,
Need your help to confirm if the LP5018 will continuous keep run the breathing feature after programming even let the host CPU enter sleep mode?
Best regards,
Albert Lee.
Part Number: LP5018 Hi,
If I want to turn the LEDs on/off individually, I think that basically it is necessary to rewrite the registers by I2C communication. Is it possible to use FETs and mechanical switches by connecting them as shown below in order…
Part Number: LP5018
This is the LED board schematics and the main board is there separately,Both are connected via the B2C connector.Let me know any changes is required in this schematics...
Part Number: LP5018 Hi,
I2C process is as following
<SDA communication flow>
1) Start bit + chip address transmission from MCU to LP5018
2) Send ACK to the MCU from LP5018
3) Register address transmission from MCU to LP5018
4) LP5018 sends…
Part Number: LP5018
As per the LP5018 datasheet It is mentioned as each channel current is set by Rref(R8=3.9K) which is connected to IREF pin,so kindly verify this schematics and confirm me the series termination resistors of 150 ohm and 100…