Part Number: LP5024 Other Parts Discussed in Thread: TLC59116 , TLC59581 , TLC5948A , TLC5957 Hi,
we currently having the tlc59116 device in our boards, while having 256 steps for the brightness.
We are looking for a similar device having 12 bit steps for…
Part Number: LP5024 Other Parts Discussed in Thread: TLC59116 , , TLC5973 , LP5009 Hi,
can you supply a bit elaborated description about how to achieve 12 bit PWM resolution, how exactly registers should be configured?
I understood that 9 bit resolution…
Part Number: LP5024 Hi
We are trying to enumerate LP5024 as I2C slave device in OS via BIOS. To do so we need to enter HW-ID.
Is the HW-Id for the slave controller = “LP5024” or “ TI LP5024” or something else? Any idea?
Thanks
-…
Part Number: LP5036 Other Parts Discussed in Thread: LP5024 LP5036 datasheet specified it support with driving dual LP5036 application, could we use LP5036 work with LP5024 together? Or we have to use the same part?
Part Number: LP5024 Hello,
Ii is my understanding that VLED should not exceed the Vout Abs Max of 6V in case of an LED short, is this correct?
Thanks,
Michael
Part Number: LP5024 Hello,
Incorporated a LP5024 on a design without doing proper investigation... Find my LP5024 using the broadcast address and the address set (ADDR0 and ADDR1 pulled down to GND)
Im using 3v3 and measure 1.7v on the vcap. LED's are common…
Part Number: LP5024 Other Parts Discussed in Thread: TLC5947 , Dear Sir/Ms.
I got customer complain about TLC5947 flicker issue.
The end customer uses the camera to take light from the TLC5947. The screen light that the user sees the camera will flicker…
Part Number: LP5024 Hi TI Team,
We are using LP5024 IC, We have the source code from the below link and we are able to successfully compile it.
Now we are trying to create sys class entries for the same for accessing the led individual color from the…