Hi Dice-K,
Sorry for late reply.
Actually, I don't have LP5569EVM on my hand since I shipped my last board to customer. So, I have to submit a request for a new EVM and it's on the way. Please forgive me some delay on this test.
BR, Jared
Part Number: BOOST-LP5569EVM Tool/software: What is the function of the 1 ohm resistor (R1 to R9) in series with the LEDs as shown in the EVM schematic. How the value is selected for the resistor to be 1 ohm. Is it to share the heat dissipation load with…
Hi Mark,
My understanding is that you want to use the internal animation engine and master fade function at the same time. Am I correct? If yes, LP5569 can't reach such function since they are different function for LP5569.
Or maybe can you directly…
Part Number: LP5569 Hi support team, I have a question about register settings.
I am gathering information from the device's D/S and EVM documents, accessing the LP5569 from the MCU via I2C, writing commands to the SRAM, and running it, but the RGB LED…
Part Number: LP5569 Other Parts Discussed in Thread: LP5813 Hi, I am searching for a way to ramp an output to a relative position. As the ramp instruction uses relative values, I don't think this is what I need. For example, I would like to change the…
Part Number: LP5569 Other Parts Discussed in Thread: LP5813 I try to LP5569's dimming
How can I run dimming??
I want the led to be dimmed by sending just one command
please check below my code.
<code>
HAL_StatusTypeDef ret; uint8_t tValue…
Part Number: LP5569 Other Parts Discussed in Thread: TEST2 Hello, I want to use LP5569 dimming control
I read all of guide but I can't.
Help me!!!
===============================================================================================
below…
Part Number: LP5569 Hi! I was considering using LP5569 to drive 3 separate segments of a 12V RGB LED strip (each segment has 3 LEDs in series for each color). Can external 12V be used to power ONLY the LEDs as long as the currents flowing into the driver…
Part Number: LP5569 Other Parts Discussed in Thread: LP5523 , Hi,
I need help regarding the control of led driver LP5569, via linux driver. We have included a kernel code for LP5569 which is similar to the kernel code of LP5523 (leds-lp5569.c), as shown…