Part Number: LP5810 Hi,
we have a I2C board which we are using to drive a led. I have made a zephyr driver for this: https://github.com/Telraam-Rear-Window-BV/LP5810-Zephyr-Driver We are now moving from a Zephyr based board to an embedded linux board…
Part Number: LP5810 Since the project is currently in the FA phase, our downstream customer needs to apply pressure/press-fit on the component surface during assembly. Therefore, we need to understand the maximum mechanical force that the component surface…
Part Number: LP5810 We are using 3 backlight LEDs display Each LED needed 20mA. all 3 connected in Parallel, we need 60mA sink current device. Can i use LP5810DDSDR? If yes, How to connect the signals. please confirm
Part Number: LP5810 Hi TI team,
On the same I2C bus we also have another device whose fixed 7-bit address is 0x51. Reads from that device return corrupted data, consistent with both devices ACKing and driving SDA simultaneously.
From datasheet, we…
Part Number: LP5810 Tool/software: Hello,
I am an FAE at a distributor that handles TI products. I received the inquiry from my customer about the LP5810. (Question) In the attached circuit, even when the 3.3V is removed (turned off), VCC does not become…
Part Number: LP5810 Tool/software: Hi, I'm using 12 LP5810 on a board to drive 12 leds, each led is driven by a single LP5810 with all output tied together. The setup works fine, but I have random crash of the LP5810.
Some units will never fail, but…
Part Number: LP5810 Tool/software: I am also interested in an I2C implementation using the LP5810. I can not seem to figure out how to use the drive linked in the related question.
Could I get some help in figuring out how to download the specified…
Part Number: LP5810 Other Parts Discussed in Thread: LP5024 Tool/software: Dear Sir,
I am planning to use the LP5810 and LP5024 ICs in my design, both of which use the I²C protocol for communication. I have the following query:
Can both the LP5810…
Part Number: LP5810 Tool/software: Hi expert,
Can the pullup rail to the SCL and SDA pins (in our case 2.2k to 1.8V) be enabled slightly before Vcc? For us the 1.8V is default on as we boot but the Vcc is from a boost and needs to be manually turned…