Part Number: LP5900 Hi Sir,
We checked LP5900 old d/s(2014) shows CDM: 200V; new d/s(2016) take away information.
It still support CDM is 200V?
Thanks, Ian.
Part Number: LP5900 Do we have any information on how much current the body diode can handle if Vout > Vin?
I have suggested that the customer use a diode from Vout to Vin to protect the body diode from an over-current condition, but I would like to…
Other Parts Discussed in Thread: LMZ23603 , LP5900 i have developed a new board where lmz23603 use to generate 5 volts.
and a sub power with LDO LP5900 to generate 1.5 volt with 5 volt VIN.
Do not work together because in LMZ data sheet you recomanded to…
Other Parts Discussed in Thread: LP5900 Hello,
I would like to use LP5900 LDO to decrease voltage from 2.87V to 2.5V. In the datasheet the Drop-Out Voltage is 80mV, so it should work... However in the "Power Supply Recommendations" it says that the Input…
Part Number: LP5900 Hi,
I'm using several of the LP5900 in my design as they have low leakage when disabled which is perfect for my battery powered application. The question is I would like to cascade (add one more level of regulation 3.1V) ahead…
Other Parts Discussed in Thread: LP5900 Hi all Would you mind if we ask LP5900? This device has the output discharge resistance. So, in case of over voltage, does this output discharge resistance operate to reduce(discharge) the voltage? Or, do you have the…
Other Parts Discussed in Thread: LP5900 Hello, I have a question about LP5900.
SNVS358R describes as follows.
"7.4.1 Operation with Enable Control" in the page-11. "However, if the application does not require the shutdown feature, the EN pin…