Part Number: LP5907-Q1 Hi all,
Can someone please provide me the input parameters necessary for FIT rate calculations based on IEC 62380? for example number of transistors inside the IC, technological structure( MOS? BICMOS?) , lambda3 classification…
Part Number: LP5907-Q1 Other Parts Discussed in Thread: LP5907 I was wondering if the enable pin of the LP5907 can be tied to the input without a pull up resistor? I am using the 3.3v output variant
Thank you!
Part Number: LP5907-Q1 Hi, Good day!
Can someone please provide me the input parameters necessary for FIT rate calculations based on IEC 62380?
for example number of transistors inside the IC, technological structure( MOS? BICMOS?) , lambda3 classification…
Part Number: LP5907-Q1 Hi,
I would like to get the best performance in the power supply for my DAC ( PCM5252 ) .
what is the effect of the clock system (in my case 50MHz ) on the power supply?
which parameters should always take into account when I'm working…
Part Number: LP5907-Q1 Dear, all
Would you mind if you ask for LP-5907-Q1?
Our customer would like to know estimated value of Short circuit current limit's deviation because they need it to design using LP-5907-Q1.
Do you know this value?
It would…
Part Number: LP5907-Q1 Hi, team
Is the upper limit of the recommended operating temperature of the LP5907-Q1 125 C? Since other Q1 grade LDO is 150 C, is it typo?
Best Regards,
Part Number: LP5907-Q1 Hi, team.
Please let me know the release date of the DQN package product of LP5907-Q1. A compact LDO with 1.8 V fixed output is required. Since it is used for mass production, it is NG in prototype.
Best Regards,
Part Number: LP5907-Q1 Dear, All
Customers are considering LP5907-Q1. The timing of Start-up is described in Figure 14. and Figure 15. on the data sheet. In this case, the time from the rising edge of EN until the output starts to rise from 0A is both about…