Part Number: LP5907-Q1 Hello,
The datasheet calls out the output capacitor ESR specified from a range of 5mOhm to 500mOhm. << image below >>
We're looking at using a ceramic capacitor which could have ESR specified as low as 2mOhm [ 10uF X7R…
Part Number: LP5907-Q1 Other Parts Discussed in Thread: LP5907
[ LP5907-Q1 ] Thermal Information Changed from Old to New Datasheet
Hi, When the LP5907-Q1 datasheet was updated from Revision B to Revision C(May 2018), thermal information was also changed…
Part Number: LP5907 Other Parts Discussed in Thread: TPS784-Q1 , TPS784 Hello TI,
I am using LP5907MFX-3.3 as the image sensor's power supply.
While using the LP5907, I would like to inquire about the output voltage waveform.
Looking at the current…
Hi ,
Yes it is possible to use LP5907-Q1 to supply the 1.2 V rail; however, you will want to consider the thermal performance depending on how much load current will be needed and how much headroom (Vin - Vout) you will have in your application. From…
Part Number: LP5907-Q1 Hi
This device does not have a reverse protection such as VIN < VOUT. However as is often the case, Vin will be go down under Vout during it is in Vin shutdown.
When it is at the above case, Vout > Vin + 0.3V (e.g. it is for…
Part Number: LP5907-Q1 Dear, All
Customers are considering LP 5907-Q1. They have questions about the operation of "Short-current Protection". In the data sheet of the device, the value of "Short circuit current limit" is written as Min 250mA …
Part Number: ADS131B04-Q1EVM Other Parts Discussed in Thread: ADS131B04-Q1 , LP5907 Hello,
I have noticed that comms with the ADS131B04Q1-EVM works more reliably (specifically the reset command) when the PHI is attached, even when the PHI is not powered…
Part Number: LP5907-Q1 Other Parts Discussed in Thread: TPS3700-Q1 Dear TI,
Can you please confirm does any short circuit protection available upon reaching current limit 500mA. Can you also confirm this IC has UV and OV protections.
We need 2V5 , 250mA…
Part Number: LP5907-Q1 Other Parts Discussed in Thread: LP5907 we use LP5907 to design for Vin:4.5V vout:3.3V/100mA,however,now we meet question is same problem board is Vout only 1.45V when the Vin is 4.5V,the Schematic diagram as below,could help give some…
Part Number: LP5907-Q1 Team,
Can you please help address my customer's questions:
Part in question:
LP5907QMFX-2.5Q1
Description
Linear Regulater VIN = 5V, Vout = 2.5
Open questions
Does the linear regulator drift over time if input voltage is…