Hi Brian,
Not yet. I will put in a request - but that may take a few days to appear.
In the mean time, the LP5910-0.9YKAR uses the same package and has the BXL file available.
They will have to edit the pin names in the generated footprint.
Hello
Just to be clear--The connection between bq24092 and Li-Ion battery should be direct with no additional components.
Between Li-Ion battery and CC2530 how to reduce the voltage from 4.2V to max of 3.9V. I would suggest a low Iq LDO, some to start…
Hi
I want to use output 47uF X7R ceramic capacitor with this part.
Also I`m using LP5910-1.0DRVR , can i use 47uF X7R ceramic capacitor? if not what is the maximum value?
Thanks
Other Parts Discussed in Thread: TPS62730 , TPS62740 , LP5910 Hi all, My customer evaluating Low Iq, Bypass mode and good light low efficiency application IOT. Vin Power source use AA battery 1.6V~3V, Vout 1.8V I suggest TPS62730, TPS62740 but not meet end…