Part Number: LP5912-Q1 Hi Experts,
Datasheet suggests that the pull-up resistor at PG pin should be 10-100kohm, can customer use 2.15kohm here? Because the PG pin is connected to the PORST pin of MCU, which has an internal 15kohm pull-down resistor…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: TPS7A88-Q1 The LP5912-Q1 Automotive 500-mA LDO look interesting , however there were some thermal issues in the datasheet that we would like to clarify:
It is mentioned that this LDO can operate…
Part Number: LP5912-Q1 Hello Sir/Ms.
The datasheet has a description of the following paragraph.
VIN = VOUT(NOM) + 0.5 V or 1.6 V, whichever is greater; VEN = 1.3 V, CIN = 1 μF, COUT = 1 μF, IOUT = 1 mA (unless otherwise
stated).(1) (2) (3)
…
Part Number: LP5912-Q1 Hi all
Our customer have a question is below. They think that θJa usually has higher thermal resistance than θJc. But the LP5912-Q1 is θJc higher thermal resistance than θJa. Is it because there is a includes two (2) thermal vias…
Part Number: LP5912-Q1 LP5912Q1.5DRVRQ1 the Datasheet show that when Vin-Vout = 0.5V is the best status。But we want 1.8V in ,1.5V out, The performance is OK?The I-out = 350mA.
Part Number: LP5912-Q1 Hello If all Ti Device without Halogen ? or how to check if this device is have Halogen or not ? did TI every device have HF(Halogen Free) Report ?
Hi Jacob,
In the process of putting this document together, I was able to locate this in the product folder. Let me know if this does not answer your need, and if so please let me know what data you are missing. The table at the bottom of page 1 gives…
Part Number: LP5912-Q1 Other Parts Discussed in Thread: TPS7A88-Q1 , Hi,
My customer is looking for a TI device with below requirements. Can you please suggest something?
This is automotive customer so please share Q1 device.
Noise requirement:…