Part Number: TPS7A26 Other Parts Discussed in Thread: LP8340 , Hi team,
custoemr need a very low Iq LDO in battery applicaiton, the spec as below:
input is 6.5V
output 3.3V
output current >500mA
they have evaluate the TPS7A26 and LP8340, they have below…
Part Number: TLV717P Other Parts Discussed in Thread: LP8340 I have problems when I try to replicate the Ground Pin Current vs Temperature graph in the datasheet and the Output Voltage vs Output Current graph in PSPICE, because in both graphs the values…
Part Number: LP8340 Hi,
Our customer wants LDO, the requirement is:
1. input voltage range is: 3V ~ 7V
2. output voltage will be adjustable or fixed voltage: 3.8V, 3.9V or 4.0V
3. the load current is 500mA
4. the Iq is less than 3uA
I select LP8340, but…
Part Number: LP8340
Hi Team, Could you tell me the value of theta ja of LP8340? I believe we should see Figure 14 (4L JEDEC Board) of the following application note but couldn't catch the value. http://www.ti.com/lit/an/snoa401r/snoa401r.pdf It seems…
Part Number: TPS746-Q1 Other Parts Discussed in Thread: LP8340 Hi team,
Do we have a AEC-Q100 p2p alternative to LD39100PURY ? I got LP8340 from bomcross but that is neither p2p nor Q1.
Best regards, Antoine
Other Parts Discussed in Thread: LP8340LP8340 requires 100uA minimum load current. To satisfy this requirement, can I reduce feedback resistor value? It is recommended 100k resistor for R2 in datasheet.
I think we satisfy minimum load current requirement…
Other Parts Discussed in Thread: LP8340 , LP38690 , LP38692 hi,
My customer need unencrypted spice model for LP8340.
I am not able to find it in TI webench spice model. Can help to share it out to me?
Rgds,
kpk
Other Parts Discussed in Thread: LP8340 Can the LP8340 linear regulator tolerate 3.3V applied to its Vout pin when the device is not powered on?
Thanks in advance!
Hi Tal,
TPS737 comes in multiple packages, as such I am unable to help with the pin to pin compatible requirement without more information. The parametric search available at ti.com/ldo is a useful tool for helping to narrow our portfolio to your specific…