Hi Partick,
Yes, so they suspect there have some test mode in LP8556 may passthough high voltage to LDO and caused damaged. Is it possible?
I will asking for the layout file to you later. thanks!
Jeff
Part Number: LP8556 Tool/software: Hi Team,
I am looking for a LED backlight driver that has similar specs to: lp8556, however do we have something newer?
Also it must be controlled by a PWM signal.
Thank you.
Kind regards,
Wouter Kragt
Part Number: LP8556 Tool/software: Hello TI,
I am trying to power a TFT screen backlight. The LEDs for the backlight are connected in parallel, requiring a forward voltage of 3.3V and a total current of 1.2A.
Is it possible to lower the LP8556 output…
Part Number: LP8556
Hello,
There is an exposed thermal pad on the WDFN package of the LP8556SQ-E09/NOPB chip.
Should-it be connected to GND or should be left unconnected?
Regards.
Sylvain
Part Number: LP8556 the formula : (CURRENT/4095) × IMAX × 20,000 × 1.2 V / RISET
But the RISET could be 12k to 100k
When the RISET is 24k , the max current/CH is 50mA
When the RISET is 14k , Is the max current/CH up to 100mA ?? or up…
Part Number: LP8556 Hi team,
I just need check the BGA package data.
Do you know t he size of the part pointed by the red arrow in the figure below is the value of the BGA electrode diameter "D"?
Thanks
Lillian
Part Number: LP8556
Hi Sir
The new project requires the use of RGB LEDs in a common anode configuration to control the brightness requirement (without color mixing functionality).
Is it possible to use the LP8556 to integrate multi-channel control for…
Part Number: LP8556 Hello,
This is a clarification to the post below:
Relevant post:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/946360/lp8556-lp8556-pwm-only/3497182?tisearch=e2e-sitesearch&keymatch=LP8556SQ…