Part Number: LP8732-Q1 Tool/software: There are two formulas to calculate ΔIL.
・Formula 2 on page 66 of the datasheet
・Formula 6 from the Application Report SLVA477B, which I was told could be referenced
I would like to use these to substitute…
Part Number: LP8732-Q1 Other Parts Discussed in Thread: PEET-GUI Tool/software: I would like to know the minimum ON time(typ and max) for the step-down DCDC.
Part Number: LP8732-Q1 Other Parts Discussed in Thread: LP87320Q1EVM Tool/software: Hi, team
About startup/shutdown delay,
What is the margin of error with respect to the set delay for each voltage system delay?
What are the possible causes? …
Part Number: LP8732-Q1 Tool/software: Hi, team
In datasheets, INPUT VOLTAGE of VIN_Bx, VANA is MIN 2.8V for Recommended Operating Conditions,
and VANA_UVLO's threshold MAX. is 2.75V (at rising).
So, When Vana is 2.75<VANA<2.8V, does the IC work…
Part Number: LP8732-Q1 Use Power IC LP873200RHDTQ1,Vin and VANA is Normal (5V Input), and EN Port is 1.8V.
But find Buck0 / Buck1 /LDO1 / LDO2 had no output.
Part Number: LP8732-Q1 Hi Ti engineer,
SCHEMATIC1 _ 04.DC Power-SOC PM.pdf
The project used TI's PMIC, LP unit test found problems;See attachment for schematic diagram
SW_B0 outputs 0.9V, and the power-off waveform after loading is strange,Load…
Part Number: LP8732-Q1 Hi team,
For LP873244-Q1, could you kindly tell me the type of 26pin GPO? Is open-drain or push-pull? My customer make it pulled up by 1.8V, but the high level is 5V. Can I2C to change it?
Thanks!
Jiawei
Part Number: LP8732-Q1 Hi Team,
Do we have part number of LP8732 44 -Q1? My customer find it from some end customer design, but I didn't find it on ti.com?
Is it SN part, or it's just a misunderstanding that we only have LP873200-Q1?
thanks…
Part Number: LP8732-Q1 Hi Auto PMIC expert:
My customer has low Iq request < 50uA for their application on PMIC solution.
They current solution is LP8732-Q1, but the Iq is 9mA that too huge.
May I know are there low Iq PMIC development plan in 2020…