Other Parts Discussed in Thread: AWR1843 , LM62440-Q1 , LM61460-Q1 , LM63635-Q1 Hello,
In our PCB we are using LP87524TRNFTQ1 PMIC IC. However, the latter works with an input voltage of approximately 5V but our circuit must be powered with an input voltage…
Part Number: LP87524B-Q1 hi TI,
IIC cannot communicate normally, MCU reads chip data, the chip does not respond, and oscilloscope waveform is normal. What is the reason? Or do you need some configuration?
See attachment for schematic diagram! LP87524.…
Part Number: LP87524J-Q1 Other Parts Discussed in Thread: LP87524-Q1 Tool/software: WEBENCH® Design Tools Hi,
I download PSpice model and try to use it to simulate on PSpice for TI. When I open simulation file, the tool show it is read only as the screenshot…
Part Number: LP87524J-Q1 Can LP87523 be used instead of LP87524? (LP87524 out of stock).
Can the LP87523 chip (3 output) be configured to be a 4 output power chip by using IIC communication? If possible, which parameters need to be configured?
Part Number: AWR6843 Hello Champs,
With below register settings, PMIC_CLKOUT of 12MHz frequency is working.
* EXTCLKSRCSEL - 0x2 (600MHz PLL)
* EXTCLK2DIV : 0x0 (div1)
* Average of MIN Div and MAX Div : 0x32 (50)
[Q1] (AWR6843) Is it possible to have…
Hi Betty,
The LP87524 may be a great fit for your system. It provides 4 DC/DC converters that can support the input and output voltage/current specifications you listed.
http://www.ti.com/product/LP87524-Q1
Regards,
Emily
Part Number: LP87524B-Q1 Other Parts Discussed in Thread: AWR1642 , AWR1843 Hi Team,
There is a good new that DIN LP87524JRNFRQ1 !
One question need you support,
For Li-ion battery used case, the normally typical voltage is 3.7V. For VIOIN of AWR1843 or…
What is being powered by the PMIC? We make recommendations based on the processor or SoC that we are powering, not a direct cross for a competitor's PMIC.
What is the input voltage?
Output current should be determined by processor requirement, because…
Part Number: LP87524B-Q1 Other Parts Discussed in Thread: TINA-TI , LP87524-Q1 Tool/software: TINA-TI or Spice Models Hello,
My customer is simulating LP87524-Q1 PSPICE model LP87524B-Q1 _TRANS.LIB.
He would like to het 0.93V/1A output at channel #2, but…